This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4M PCIE clock



HI

Refer to spec the PCIE clock can refer to HFOSC_CLK if it is one of 19.2,20,24,25,26,27,31,25,100 MHz, so we also can remove external clock generator,right? 

Thanks a lot

B.R

Y.L

  • Hi YuLin,

    Yes, Serdes can generate the 100-MHz clock needed for PCIe operation. The list of clocks you mentioned is the reference clock for Serdes internal PLL. Software must configure all muxes and PLLs for PCIe mode (100-MHz clock out).

    Note that the 100-MHz PCIe clock distribution (on the PCB) must be carefully evaluated. Please refer to PCIe standard specs for the 100-MHz clock distribution variants.

    Regards,

    Stan