This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA756: System files become read-only

Part Number: DRA756

At present, our J6 project USES 8G EMMC. At present, we set the system file to read and write by default. During the process of testing switch or reading and writing to the file, the system file will become read-only.

  • Hi

    Can you attach the complete console logs

    Please check if you see any errors being reported for IO operations to EMMC

    You can get the complete kernel logs using the command below

    # dmesg

  • 1、The attachment is the log of the exception #dmesg;

    2、 if you see any errors being reported for IO operations to EMMC?What is this? What IO?

    3、Modify the J6 system fstab file to mount the root directory as read-only after the system is started. After repeatedly running up and down for a period of time, there will be an error when executing "fsck.ext4-p /dev/mmcblk0p1". The information is as follows:

    root@dra7xx-evm:~# fsck.ext4 -p /dev/mmcblk0p1

    rootfs contains a file system with errors, check forced.

    rootfs: 3470/7168 files (0.0% non-contiguous), 21493/28672 blocks

    What are the possible reasons for this, and how do you find them in terms of software and hardware?

    root@dra7xx-evm:~# 
    root@dra7xx-evm:~# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 3.14.63 (root@ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #80 SMP PREEMPT Tue Oct 23 02:07:32 PDT 2018
    [    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] Truncating memory at 0x80000000 to fit in 32-bit physical address space
    [    0.000000] Machine model: TI DRA742
    [    0.000000] Reserved memory: created CMA memory pool at 0x94000000, size 80 MiB
    [    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x99000000, size 64 MiB
    [    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x9d000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x9f000000, size 16 MiB
    [    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0xa8000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node cmem@A6000000, compatible id shared-dma-pool
    [    0.000000] cma: CMA: reserved 24 MiB at ae000000
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] On node 0 totalpages: 515839
    [    0.000000] free_area_init_node: node 0, pgdat c097f280, node_mem_map ecf8e000
    [    0.000000]   Normal zone: 1520 pages used for memmap
    [    0.000000]   Normal zone: 0 pages reserved
    [    0.000000]   Normal zone: 186368 pages, LIFO batch:31
    [    0.000000]   HighMem zone: 2576 pages used for memmap
    [    0.000000]   HighMem zone: 329471 pages, LIFO batch:31
    [    0.000000] DRA752 ES2.0
    [    0.000000] PERCPU: Embedded 8 pages/cpu @ecf47000 s8704 r8192 d15872 u32768
    [    0.000000] pcpu-alloc: s8704 r8192 d15872 u32768 alloc=8*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 514319
    [    0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=/dev/mmcblk0p1 rw rootfstype=ext4 rootwait
    [    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 1453752K/2063356K available (6391K kernel code, 675K rwdata, 2252K rodata, 372K init, 255K bss, 609604K reserved, 1317884K highmem)
    [    0.000000] Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
        vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
        lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0xc0008000 - 0xc08790a4   (8645 kB)
          .init : 0xc087a000 - 0xc08d7200   ( 373 kB)
          .data : 0xc08d8000 - 0xc0980f10   ( 676 kB)
           .bss : 0xc0980f1c - 0xc09c0bfc   ( 256 kB)
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [    0.000030] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65536000000000ns
    [    0.000030] OMAP clocksource: 32k_counter at 32768 Hz
    [    0.000427] Architected cp15 timer(s) running at 6.14MHz (virt).
    [    0.000462] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 2794592043008ns
    [    0.000470] Switching to timer-based delay loop
    [    0.001472] Console: colour dummy device 80x30
    [    0.001488] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.001494] This ensures that you still see kernel messages. Please
    [    0.001500] update your kernel commandline.
    [    0.001515] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [    0.001528] pid_max: default: 32768 minimum: 301
    [    0.001643] Security Framework initialized
    [    0.001692] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001703] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.025028] Initializing cgroup subsys net_cls
    [    0.025063] CPU: Testing write buffer coherency: ok
    [    0.025316] /cpus/cpu@0 missing clock-frequency property
    [    0.025352] /cpus/cpu@1 missing clock-frequency property
    [    0.025363] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.025387] Setting up static identity map for 0x80644068 - 0x806440d8
    [    0.080806] CPU1: Booted secondary processor
    [    0.080835] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.080964] Brought up 2 CPUs
    [    0.080980] SMP: Total of 2 processors activated (24.59 BogoMIPS).
    [    0.080986] CPU: All CPU(s) started in SVC mode.
    [    0.081404] devtmpfs: initialized
    [    0.081999] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.083745] omap_hwmod: l3_main_2 using broken dt data from ocp
    [    0.097346] omap_hwmod: tptc0 using broken dt data from edma-controller
    [    0.097883] omap_hwmod: tptc1 using broken dt data from edma-controller
    [    0.192454] omap_hwmod: dcan1: _wait_target_disable failed
    [    0.291564] pinctrl core: initialized pinctrl subsystem
    [    0.292304] regulator-dummy: no parameters
    [    0.296652] NET: Registered protocol family 16
    [    0.298451] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.300519] cpuidle: using governor ladder
    [    0.300528] cpuidle: using governor menu
    [    0.347327] syscon 4a002000.tisysconcore: regmap [mem 0x4a002000-0x4a0026cf] registered
    [    0.347664] syscon 4a002e00.tisyscon: regmap [mem 0x4a002e00-0x4a002e7b] registered
    [    0.350262] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
    [    0.350515] OMAP GPIO hardware version 0.1
    [    0.351239] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
    [    0.352067] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
    [    0.352905] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
    [    0.353771] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
    [    0.354673] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
    [    0.355565] gpiochip_add: registered GPIOs 192 to 223 on device: gpio
    [    0.356475] gpiochip_add: registered GPIOs 224 to 255 on device: gpio
    [    0.363665] platform 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
    [    0.383126] No ATAGs?
    [    0.383154] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.383163] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.385917] OMAP DMA hardware revision 0.0
    [    0.412112] bio: create slab <bio-0> at 0
    [    0.427130] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
    [    0.434160] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
    [    0.434758] of_get_named_gpiod_flags exited with status 0
    [    0.435006] evm_3v3_sd: 3300 mV 
    [    0.435140] of_get_named_gpiod_flags exited with status 0
    [    0.435367] evm_3v3_sd4: 3300 mV 
    [    0.435482] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-evm_3v3_sw[0]'
    [    0.435686] evm_3v3_sw: 3300 mV 
    [    0.435790] of_get_named_gpiod_flags: can't parse gpios property of node '/fixedregulator-aic_dvdd[0]'
    [    0.436003] aic_dvdd: 1800 mV 
    [    0.436061] aic_dvdd: supplied by evm_3v3_sw
    [    0.436204] of_get_named_gpiod_flags exited with status 0
    [    0.436417] vtt_fixed: 1350 mV 
    [    0.439892] vgaarb: loaded
    [    0.440346] i2c-core: driver [palmas] using legacy suspend method
    [    0.440355] i2c-core: driver [palmas] using legacy resume method
    [    0.440970] SCSI subsystem initialized
    [    0.441413] libata version 3.00 loaded.
    [    0.442247] usbcore: registered new interface driver usbfs
    [    0.442412] usbcore: registered new interface driver hub
    [    0.442596] usbcore: registered new device driver usb
    [    0.444893] palmas 0-0058: IRQ missing: skipping irq request
    [    0.445226] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
    [    0.445367] prom_parse: Bad cell count for /ocp/i2c@48070000/tps659038@58
    [    0.447435] smps123: 850 <--> 1500 mV at 1080 mV 
    [    0.449047] smps45: 850 <--> 1500 mV at 990 mV 
    [    0.450644] smps6: 850 <--> 1500 mV at 1080 mV 
    [    0.453723] smps7: 850 <--> 1500 mV at 1060 mV 
    [    0.455338] smps8: 850 <--> 1500 mV at 1010 mV 
    [    0.456758] smps9: 1800 mV 
    [    0.461247] ldo1: 1800 <--> 3300 mV at 3000 mV 
    [    0.471485] ldo2: 3300 mV 
    [    0.481117] ldo3: 1800 mV 
    [    0.481963] LDO4: at 1800 mV 
    [    0.482556] LDO5: no parameters
    [    0.483154] LDO6: no parameters
    [    0.483742] LDO7: no parameters
    [    0.484321] LDO8: no parameters
    [    0.491148] ldo9: 1050 mV 
    [    0.501236] ldoln: 1800 mV 
    [    0.511163] ldousb: 3300 mV 
    [    0.511852] REGEN1: no parameters
    [    0.512365] regen2: no parameters
    [    0.512939] sysen1: no parameters
    [    0.513507] sysen2: no parameters
    [    0.513768] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
    [    0.514239] pps_core: LinuxPPS API ver. 1 registered
    [    0.514248] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.514363] PTP clock support registered
    [    0.515664] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
    [    0.515941] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
    [    0.516773] omap-iommu 40d01000.mmu: 40d01000.mmu registered
    [    0.516882] omap-iommu 40d02000.mmu: 40d02000.mmu registered
    [    0.516985] omap-iommu 55082000.mmu: 55082000.mmu registered
    [    0.518245] NetLabel: Initializing
    [    0.518255] NetLabel:  domain hash size = 128
    [    0.518262] NetLabel:  protocols = UNLABELED CIPSOv4
    [    0.518313] NetLabel:  unlabeled traffic allowed by default
    [    0.518808] Switched to clocksource arch_sys_counter
    [    0.537976] NET: Registered protocol family 2
    [    0.538679] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.538744] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.538897] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.538941] TCP: reno registered
    [    0.538954] UDP hash table entries: 512 (order: 2, 16384 bytes)
    [    0.538985] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    [    0.539179] NET: Registered protocol family 1
    [    0.539443] RPC: Registered named UNIX socket transport module.
    [    0.539453] RPC: Registered udp transport module.
    [    0.539460] RPC: Registered tcp transport module.
    [    0.539466] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.539476] PCI: CLS 0 bytes, default 64
    [    0.540521] hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
    [    0.541016] yt_initio_probe
    [    0.541106] gpio-105 (CPU_EN_12VCAME): gpiod_request: status -16
    [    0.543940] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.634517] bounce pool size: 64 pages
    [    0.634789] VFS: Disk quotas dquot_6.5.2
    [    0.634897] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.635507] NFS: Registering the id_resolver key type
    [    0.635541] Key type id_resolver registered
    [    0.635550] Key type id_legacy registered
    [    0.635582] jffs2: version 2.2. (NAND) (SUMMARY)  \xffffffc2\xffffffa9 2001-2006 Red Hat, Inc.
    [    0.635762] msgmni has been set to 697
    [    0.639692] alg: No test for stdrng (krng)
    [    0.639876] NET: Registered protocol family 38
    [    0.639904] io scheduler noop registered
    [    0.639913] io scheduler deadline registered
    [    0.639946] io scheduler cfq registered (default)
    [    0.646139] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
    [    0.649042] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/axi@0/pcie@51000000[0]'
    [    0.684618] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
    [    0.684633] pci_bus 0000:00: root bus resource [io  0x1000-0x10000]
    [    0.684645] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
    [    0.684656] pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
    [    0.684694] pci 0000:00:00.0: [104c:8888] type 01 class 0x060400
    [    0.684726] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
    [    0.684749] pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x0000ffff]
    [    0.684806] pci 0000:00:00.0: supports D1
    [    0.684816] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
    [    0.685170] PCI: bus0: Fast back to back transfers disabled
    [    0.685409] PCI: bus1: Fast back to back transfers enabled
    [    0.685424] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
    [    0.685438] pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01
    [    0.685526] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
    [    0.685542] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
    [    0.685555] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    0.685575] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    0.685591] pci_bus 0000:00: resource 4 [io  0x1000-0x10000]
    [    0.685601] pci_bus 0000:00: resource 5 [mem 0x20013000-0x2fffffff]
    [    0.689792] pbias_mmc_omap5: 1800 <--> 3000 mV at 3000 mV 
    [    0.690548] abb_mpu: 1100 <--> 1210 mV 
    [    0.690924] abb_ivahd: 1060 <--> 1250 mV 
    [    0.691281] abb_dspeve: 1060 <--> 1250 mV 
    [    0.691639] abb_gpu: 1060 <--> 1280 mV 
    [    0.692753] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.696683] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@4806a000[0]'
    [    0.697074] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
    [    1.714771] console [ttyS0] enabled
    [    1.718736] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48020000[0]'
    [    1.719157] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 300, base_baud = 3000000) is a 8250
    [    1.728369] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/serial@48422000[0]'
    [    1.728735] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 301, base_baud = 3000000) is a 8250
    [    1.739295] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
    [    1.746448] [drm] Initialized drm 1.1.0 20060810
    [    1.761631] brd: module loaded
    [    1.770189] loop: module loaded
    [    1.773661] (hci_tty): inside hci_tty_init
    [    1.778129] (hci_tty): allocated 250, 0
    [    1.784385] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
    [    1.791157] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [    1.799742] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst 
    [    1.810233] scsi0 : ahci_platform
    [    1.814049] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 334
    [    1.823321] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    1.835806] m25p80 spi32766.0: found w25q128, expected s25fl256s1
    [    1.842056] m25p80 spi32766.0: w25q128 (16384 Kbytes)
    [    1.851026] libphy: Fixed MDIO Bus: probed
    [    1.856457] PPP generic driver version 2.4.2
    [    1.861278] usbcore: registered new interface driver asix
    [    1.866842] usbcore: registered new interface driver ax88179_178a
    [    1.873134] usbcore: registered new interface driver cdc_ether
    [    1.879166] usbcore: registered new interface driver smsc95xx
    [    1.885074] usbcore: registered new interface driver net1080
    [    1.890914] usbcore: registered new interface driver cdc_subset
    [    1.896996] usbcore: registered new interface driver zaurus
    [    1.902785] usbcore: registered new interface driver cdc_ncm
    [    1.909250] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    1.915807] ehci-pci: EHCI PCI platform driver
    [    1.920439] ehci-omap: OMAP-EHCI Host Controller driver
    [    1.926109] usbcore: registered new interface driver cdc_wdm
    [    1.931977] usbcore: registered new interface driver usb-storage
    [    1.938312] usbcore: registered new interface driver usbserial
    [    1.944323] usbcore: registered new interface driver usbserial_generic
    [    1.951028] usbserial: USB Serial support registered for generic
    [    1.957195] usbcore: registered new interface driver option
    [    1.962941] usbserial: USB Serial support registered for GSM modem (1-port)
    [    1.971070] mousedev: PS/2 mouse device common for all mice
    [    1.978958] i2c-core: driver [rtc-ds1307] using legacy suspend method
    [    1.985430] i2c-core: driver [rtc-ds1307] using legacy resume method
    [    1.992472] rtc rtc0: 48838000.rtcss: dev (254:0)
    [    1.992496] omap_rtc 48838000.rtcss: rtc core: registered 48838000.rtcss as rtc0
    [    2.000783] i2c /dev entries driver
    [    2.004657] Driver for 1-wire Dallas network protocol.
    [    2.010930] coproc iva_coproc: probe
    [    2.014644] Adding alias for supply vdd,iva_coproc -> vdd,4a0025cc.voltdm
    [    2.021482] Adding alias for supply vbb,iva_coproc -> vbb,4a0025cc.voltdm
    [    2.029522] coproc iva_coproc: coproc_probe result=0
    [    2.034547] coproc dsp_coproc: probe
    [    2.038223] Adding alias for supply vdd,dsp_coproc -> vdd,4a0025e0.voltdm
    [    2.045169] Adding alias for supply vbb,dsp_coproc -> vbb,4a0025e0.voltdm
    [    2.053080] coproc dsp_coproc: coproc_probe result=0
    [    2.063006] of_get_named_gpiod_flags exited with status 0
    [    2.063018] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@4809c000[0]'
    [    2.099063] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480b4000[0]'
    [    2.099074] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480b4000[0]'
    [    2.139031] of_get_named_gpiod_flags exited with status 0
    [    2.139042] of_get_named_gpiod_flags: can't parse gpios property of node '/ocp/mmc@480d1000[0]'
    [    2.168850] ata1: SATA link down (SStatus 0 SControl 300)
    [    2.179483] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.185814] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
    [    2.188873] mmc1: BKOPS_EN bit is not set
    [    2.199037] mmc1: new high speed DDR MMC card at address 0001
    [    2.205313] mmcblk0: mmc1:0001 MMC08G 7.26 GiB 
    [    2.210121] mmcblk0boot0: mmc1:0001 MMC08G partition 1 4.00 MiB
    [    2.216359] mmcblk0boot1: mmc1:0001 MMC08G partition 2 4.00 MiB
    [    2.228191]  mmcblk0: p1 p2 p3 p4 p5 p6 p7
    [    2.233683] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
    [    2.240712] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
    [    2.246501]  mmcblk0boot1: unknown partition table
    [    2.252430]  mmcblk0boot0: unknown partition table
    [    2.257365] alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100
    [    2.265011] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
    [    2.273110] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
    [    2.285918] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
    [    2.291754] omap-sham 4b101000.sham: initialization failed.
    [    2.297379] omap-sham: probe of 4b101000.sham failed with error -22
    [    2.304362] usbcore: registered new interface driver usbhid
    [    2.310045] usbhid: USB HID core driver
    [    2.315784] extcon-usb-gpio extcon_usb1: GPIO lookup for consumer id
    [    2.315796] extcon-usb-gpio extcon_usb1: using device tree for GPIO lookup
    [    2.315807] of_get_named_gpiod_flags: can't parse gpios property of node '/extcon_usb1[0]'
    [    2.315817] extcon-usb-gpio extcon_usb1: using lookup tables for GPIO lookup
    [    2.315826] extcon-usb-gpio extcon_usb1: lookup for GPIO id failed
    [    2.315836] extcon-usb-gpio extcon_usb1: GPIO lookup for consumer vbus
    [    2.315845] extcon-usb-gpio extcon_usb1: using device tree for GPIO lookup
    [    2.315854] of_get_named_gpiod_flags: can't parse gpios property of node '/extcon_usb1[0]'
    [    2.315862] extcon-usb-gpio extcon_usb1: using lookup tables for GPIO lookup
    [    2.315871] extcon-usb-gpio extcon_usb1: lookup for GPIO vbus failed
    [    2.316099] extcon-usb-gpio extcon_usb1: extcon_usb1 node name: OTG
    [    2.322667] extcon-usb-gpio extcon_usb2: GPIO lookup for consumer id
    [    2.322678] extcon-usb-gpio extcon_usb2: using device tree for GPIO lookup
    [    2.322688] of_get_named_gpiod_flags: can't parse gpios property of node '/extcon_usb2[0]'
    [    2.322697] extcon-usb-gpio extcon_usb2: using lookup tables for GPIO lookup
    [    2.322706] extcon-usb-gpio extcon_usb2: lookup for GPIO id failed
    [    2.322716] extcon-usb-gpio extcon_usb2: GPIO lookup for consumer vbus
    [    2.322724] extcon-usb-gpio extcon_usb2: using device tree for GPIO lookup
    [    2.322733] of_get_named_gpiod_flags: can't parse gpios property of node '/extcon_usb2[0]'
    [    2.322741] extcon-usb-gpio extcon_usb2: using lookup tables for GPIO lookup
    [    2.322749] extcon-usb-gpio extcon_usb2: lookup for GPIO vbus failed
    [    2.322972] extcon-usb-gpio extcon_usb2: extcon_usb1 node name: HOST
    [    2.329802] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
    [    2.336411] ip_tables: (C) 2000-2006 Netfilter Core Team
    [    2.341858] TCP: cubic registered
    [    2.345189] Initializing XFRM netlink socket
    [    2.349555] NET: Registered protocol family 17
    [    2.354039] NET: Registered protocol family 15
    [    2.358575] Bridge firewalling registered
    [    2.362667] 8021q: 802.1Q VLAN Support v1.8
    [    2.366912] Key type dns_resolver registered
    [    2.371789] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
    [    2.378088] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
    [    2.385976] Power Management for TI OMAP4+ devices.
    [    2.391055] ThumbEE CPU extension supported.
    [    2.395349] Registering SWP/SWPB emulation handler
    [    2.400172] SmartReflex Class3 initialized
    [    2.405965] aic_dvdd: disabling
    [    2.409147] evm_3v3_sd4: disabling
    [    2.412560] evm_3v3_sd: disabling
    [    2.415887] regulator-dummy: disabling
    [    2.419916] dmm 4e000000.dmm: workaround for errata i878 in use
    [    2.427570] dmm 4e000000.dmm: initialized all PAT entries
    [    2.434672] omap_rtc 48838000.rtcss: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
    [    2.443505] sr_init: No PMIC hook to init smartreflex
    [    2.448794] sr_init: platform driver register failed for SR
    [    2.468611] EXT4-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended
    [    2.498359] EXT4-fs (mmcblk0p1): mounted filesystem without journal. Opts: (null)
    [    2.505906] VFS: Mounted root (ext4 filesystem) on device 179:1.
    [    2.512359] devtmpfs: mounted
    [    2.731574] EXT4-fs (mmcblk0p6): recovery complete
    [    2.736402] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)
    [    2.750240] EXT4-fs (mmcblk0p7): recovery complete
    [    2.755061] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
    [    2.790467] pinctrl-single 4a003400.pinmux: bad data for mux cpsw_default
    [    2.797293] pinctrl-single 4a003400.pinmux: no pins entries for cpsw_default
    [    2.805431] cpsw_phy_sel_probe:hzk gpio_request 51(GPIO2_19)
    [    2.821427] cpsw 48484000.ethernet: Detected MACID = 88:3f:4a:7e:90:94
    [    2.829085] cpsw 48484000.ethernet: cpsw: Detected MACID = 00:2c:70:ec:90:a9
    [    2.884230] udevd[1077]: starting version 182
    [    2.951476] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null)
    [    3.018839] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
    [    3.024970] davinci_mdio 48485000.mdio: detected phy mask fffffffe
    [    3.036536] libphy: 48485000.mdio: probed
    [    3.040595] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, id 0x600d8595, driver Broadcom BCM54210S
    [    3.056607]  remoteproc0: 40800000.dsp is available
    [    3.061603]  remoteproc0: Note: remoteproc is still under development and considered experimental.
    [    3.070626]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    3.096519]  remoteproc0: registered virtio0 (type 7)
    [    3.103172] can: controller area network core (rev 20120528 abi 9)
    [    3.109625] NET: Registered protocol family 29
    [    3.118904]  remoteproc0: powering up 40800000.dsp
    [    3.124838] CAN device driver interface
    [    3.129808]  remoteproc0: Booting fw image dra7-dsp1-fw.xe66, size 948568
    [    3.143163] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
    [    3.149052] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
    [    3.154960] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
    [    3.162826] can: raw protocol (rev 20120528)
    [    3.202243] omap_hwmod: dcan1: _wait_target_disable failed
    [    3.213599] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=348)
    [    3.228384] c_can_platform 48480000.can: c_can_platform device registered (regs=f04c8000, irq=349)
    [    3.229685]  remoteproc0: remote processor 40800000.dsp is now up
    [    3.245092] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    3.256096] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x36
    [    3.270874] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x37
    [    3.280505] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
    [    3.292049] rpmsg_rpc rpmsg2: probing service rpmsg-dce-dsp with src 1024 dst 101
    [    3.303790] rpmsg_rpc rpmsg2: published functions = 8
    [    3.306943] c_can_platform 4ae3c000.can can0: setting BTR=1c04 BRPE=0000
    [    3.322964] c_can_platform 48480000.can can1: setting BTR=1c04 BRPE=0000
    [    3.763748] dwc3 48890000.usb: otg: primary host xhci-hcd.0.auto registered
    [    3.770760] dwc3 48890000.usb: otg: shared host xhci-hcd.0.auto registered
    [    3.777664] dwc3 48890000.usb: otg: can't start till gadget registers
    [    4.185274] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [    4.191022] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
    [    4.199037] xhci-hcd xhci-hcd.1.auto: irq 424, io mem 0x488d0000
    [    4.205195] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    4.212025] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.219290] usb usb1: Product: xHCI Host Controller
    [    4.224187] usb usb1: Manufacturer: Linux 3.14.63 xhci-hcd
    [    4.229706] usb usb1: SerialNumber: xhci-hcd.1.auto
    [    4.235129] hub 1-0:1.0: USB hub found
    [    4.238945] hub 1-0:1.0: 1 port detected
    [    4.243120] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [    4.248841] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
    [    4.256672] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
    [    4.263502] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.270768] usb usb2: Product: xHCI Host Controller
    [    4.275665] usb usb2: Manufacturer: Linux 3.14.63 xhci-hcd
    [    4.281180] usb usb2: SerialNumber: xhci-hcd.1.auto
    [    4.286605] hub 2-0:1.0: USB hub found
    [    4.290409] hub 2-0:1.0: 1 port detected
    [    4.463763] random: mkfs.ext4 urandom read with 89 bits of entropy available
    [    4.520289] udc 48890000.usb: registering UDC driver [g_mass_storage]
    [    4.520320] Number of LUNs=8
    [    4.528731] Mass Storage Function, version: 2009/09/11
    [    4.539537] LUN: removable file: (no medium)
    [    4.546730] Number of LUNs=1
    [    4.549723] lun0: open backing file: /mnt/ramdrive/ext4-file
    [    4.549735] LUN: file: /mnt/ramdrive/ext4-file
    [    4.554194] Number of LUNs=1
    [    4.557095] g_mass_storage gadget: adding config #1 'Linux File-Backed Storage'/bf0da39c
    [    4.557166] g_mass_storage gadget: I/O thread pid: 1134
    [    4.557180] g_mass_storage gadget: adding 'Mass Storage Function'/ec776e00 to config 'Linux File-Backed Storage'/bf0da39c
    [    4.557199] g_mass_storage gadget: cfg 1/bf0da39c speeds: super high full
    [    4.557207] g_mass_storage gadget:   interface 0 = Mass Storage Function/ec776e00
    [    4.557218] g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
    [    4.564302] g_mass_storage gadget: userspace failed to provide iSerialNumber
    [    4.568907] usb 1-1: new high-speed USB device number 2 using xhci-hcd
    [    4.577969] g_mass_storage gadget: g_mass_storage ready
    [    4.583265] dwc3 48890000.usb: otg: gadget gadget registered
    [    4.588995] g_mass_storage gadget: usb_gadget_start
    [    4.589015] g_mass_storage 48890000.usb: usb_gadget_udc_start
    [    4.591456] g_mass_storage gadget: usb_gadget_stop
    [    4.591495] g_mass_storage 48890000.usb: usb_gadget_udc_stop
    [    4.591590] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.598396] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 3
    [    4.608899] xhci-hcd xhci-hcd.0.auto: irq 423, io mem 0x48890000
    [    4.617012] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002
    [    4.626090] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.633533] usb usb3: Product: xHCI Host Controller
    [    4.639001] usb usb3: Manufacturer: Linux 3.14.63 xhci-hcd
    [    4.644520] usb usb3: SerialNumber: xhci-hcd.0.auto
    [    4.651008] hub 3-0:1.0: USB hub found
    [    4.654803] hub 3-0:1.0: 1 port detected
    [    4.659582] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.667970] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 4
    [    4.677404] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003
    [    4.685641] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.693120] usb usb4: Product: xHCI Host Controller
    [    4.698023] usb usb4: Manufacturer: Linux 3.14.63 xhci-hcd
    [    4.704798] usb usb4: SerialNumber: xhci-hcd.0.auto
    [    4.710650] hub 4-0:1.0: USB hub found
    [    4.714444] hub 4-0:1.0: 1 port detected
    [    4.729490] usb 1-1: New USB device found, idVendor=02e3, idProduct=0702
    [    4.736228] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
    [    4.744732] usb 1-1: Product: 35549
    [    4.748882] usb 1-1: Manufacturer: 355
    [    4.753632] usb-storage 1-1:1.0: USB Mass Storage device detected
    [    4.761770] scsi1 : usb-storage 1-1:1.0
    [    5.503375] net eth0: initializing cpsw version 1.15 (0)
    [    5.591647] bcm54210s_config_init:hzk read1 RDB MODE_CONTROL=0x7e1c
    [    5.597945] bcm54210s_config_init:hzk write RDB MODE_CONTROL=0x7e1b
    [    5.608288] bcm54210s_config_init:hzk read2 RDB MODE_CONTROL=0x7f1b
    [    5.616608] bcm54210s_config_init:hzk read1 RDB COPPER_MISCELLANEOUS_CONTROL=0x7167
    [    5.624310] bcm54210s_config_init:hzk write RDB COPPER_MISCELLANEOUS_CONTROL=0x71e7
    [    5.635847] bcm54210s_config_init:hzk read2 RDB COPPER_MISCELLANEOUS_CONTROL=0x71e7
    [    5.643556] net eth0: phy found : id is : 0x600d8595
    [    5.648652] cpsw_gmii_sel_dra7xx:hzk reg=3322 addr=fc002554
    [    5.659925] 8021q: adding VLAN 0 to HW filter on device eth0
    [    5.759327] scsi 1:0:0:0: Direct-Access     XDJA     Flash Disk       1.01 PQ: 0 ANSI: 4
    [    5.775687] sd 1:0:0:0: [sda] 4294967295 512-byte logical blocks: (2.19 TB/1.99 TiB)
    [    5.784730] sd 1:0:0:0: [sda] Test WP failed, assume Write Enabled
    [    5.792066] sd 1:0:0:0: Attached scsi generic sg0 type 0
    [    5.797564] sd 1:0:0:0: [sda] Cache data unavailable
    [    5.802923] sd 1:0:0:0: [sda] Assuming drive cache: write through
    [    5.811279] sd 1:0:0:0: [sda] Test WP failed, assume Write Enabled
    [    5.819265] sd 1:0:0:0: [sda] Cache data unavailable
    [    5.824402] sd 1:0:0:0: [sda] Assuming drive cache: write through
    [    5.834334] random: nonblocking pool is initialized
    [    5.842670]  sda: sda1
    [    5.846782] sd 1:0:0:0: [sda] Test WP failed, assume Write Enabled
    [    5.854963] sd 1:0:0:0: [sda] Cache data unavailable
    [    5.860547] sd 1:0:0:0: [sda] Assuming drive cache: write through
    [    5.868709] sd 1:0:0:0: [sda] Attached SCSI removable disk
    [    7.645657] libphy: 48485000.mdio:00 - Link is Up - 1000/Full
    [  612.582822] EXT4-fs error (device mmcblk0p1): __ext4_new_inode:987: comm touch: failed to insert inode 3424: doubly allocated?
    [  612.595423] EXT4-fs (mmcblk0p1): Remounting filesystem read-only
    

  • HI

    is the issue seen on multiple boards or is it specifically seen when you run your tests on a particular board

    You may additionally check if the issue goes away on a subsequent reflash  of the emmc and  clean restart of the system.

    If you are rebooting the board several times as part of your testing, ensure that the system shutdown is graceful, then the contents of the filesystem will stay consistent.

    If you are asynchronously shutting down your board, you may have to run additional fsck type checks to ensure that the filesystem contents are not corrupted from a previous shutdown

  • HI,

    1、is the issue seen on multiple boards or is it specifically seen when you run your tests on a particular board?

    repaly:All the boards can be reproduced; Follow this experiment: power up and down frequently, and read and write to EMMC

    2、You may additionally check if the issue goes away on a subsequent reflash  of the emmc and  clean restart of the system

    repaly:The problem will not go away after reading only, unless you use the following command to fix it:fsck.ext4 –p /dev/mmcblk0p1;

    3、If you are rebooting the board several times as part of your testing, ensure that the system shutdown is graceful, then the contents of the filesystem will stay consistent.

    repaly:System shutdown reasonable how to understand? We start at 30S and close at 30S;

    4、If you are asynchronously shutting down your board, you may have to run additional fsck type checks to ensure that the filesystem contents are not corrupted from a previous shutdown

    repaly:How to understand asynchronously shutting down your board?How is the normal shutdown software handled?

    We will now mount the following program at boot time, forcing it to be read-only, but the following error will still occur:"rootfs was not cleanly unmounted, check forced."(Mount changes place:/etc/init.d/checkroot.sh)

    This error occurred earlier:"rootfs contains a file system with errors, check forced."

    Help to analyze the causes? THS!

  • Hi

     you need to ensure that you following one of the following

    1. Use shutdown command to ensure that the file system state is cleanly updated as against an abrupt power down of the board

    2. If as part of your tests, if you have any writes to the file system, ensure you either flush or unmount the filesystem cleanly before powering down

    if you do not gracefully shutdown, filesystem state can be corrupted and will require fsck to rescan and fix errors

  • HI:
         

    1、We found that there were also errors in constantly switching on and then frequently reading and writing; There is no power cut;

    2、If all power is suddenly cut off, is there no way to process the data before the cut off?

    3、We now find that frequent reads and writes to media files are fine, while errors occur to system files;

    What is the difference between the two files?

    4、We will now mount the following program at boot time, forcing it to be read-only, but the following error will still occur:"rootfs was not cleanly unmounted, check forced."(Mount changes place:/etc/init.d/checkroot.sh);We wanted to start before changing read-only, but there was still an error。While we can burn the new image file (change read-only) without any problem, what's the difference

  • Hi

    to simplify the discussion, anytime you shutdown the system (power abruptly going off, you switching off the power switch), the filesystem state can be left in unclean state.

    If instead we follow the right steps to gracefully shutdown (typically using the shutdown command  or similar), then the applications that were running are stopped first and any dirty filesystem updates are flushed to the disk before disabling the storage device

    If you are not gracefully shutting down, it is possible that the filesystem state on the next reboot is scanned for and any errors identified flagged. You then run fsck to correct these

    Depending on your end application and criticality of the data, you may need other external means(on board capacitor to keep the board powered on for short while longer to allow for graceful shutdown)

    On difference between user data vs system files, i dont have specific feedback. It is possible that some scripts in the filesystem where running and accessing content from the filesystem while the shutdown happened

    Overall, if you are not doing a graceful shutdown it is inevitable that we see errors being reported on reboot.