Part Number: PROCESSOR-SDK-AM65X
Other Parts Discussed in Thread: DA8XX
Hello TI Team,
We are working on a custom platform based on TI's AM65X SOC.
There is a usecase where we need to check GPIO1_57 value in U-boot. But somehow we are not able to access GPIO's from the u-boot.
we have followed a method from one of the TI's previous thread : 
But we are not able to get desired output.
Below are the changes we made in accordance with the above URL.
u-boot/arch/arm/dts/k3-am65-main.dtsi
&cbass_main {
.....
main_i2c3: i2c@2030000 {
....
};
main_gpio1: main_gpio1@601000 {
compatible = "ti,k2g-gpio", "ti,keystone-gpio";
reg = <0x0 0x601000 0x0 0x100>;
gpio-controller;
#gpio-cells = <2>;
ti,ngpio = <90>;
ti,davinci-gpio-unbanked = <0>;
clocks = <&k3_clks 58 0>;
clock-names = "gpio";
};
u-boot/arch/arm/dts/k3-am654-base-board.dts
&main_pmx0 {
main_gpio1_pins_default: main-gpio1-pins-default {
pinctrl-single,pins = <
AM65X_IOPAD(0x0264, PIN_INPUT, 0) /* (W27)GPIO1_57 */
>;
};
&main_gpio1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_gpio1_pins_default>;
};
The below is the code that we are using for the accessing the GPIO in u-boot.
tmp = gpio_request(209,"lcd_det"); /*GPIO1_57*/
if(tmp<0)
{
printf("Mistral GPIO_209 Request fail \n");
}
tmp = gpio_direction_input(209);
if(tmp<0)
{
printf("Mistral GPIO_209 direction fail \n");
}
tmp = gpio_get_value(209);
if(tmp<0)
{
printf("Mistral GPIO_209 get_value fail \n");
}
We are seeing that the gpio request itself is failing with the above code changes.
By using "md" and "mw" commands in u-boot we are able to read this perticular GPIO.
Requesting your support on this issue that we are facing.
Regards,
Ramakrishna