Part Number: TMS320C6416T
Other Parts Discussed in Thread: TMS320C6713B
Tool/software: TI C/C++ Compiler
Hi,
I've created this thread clicking at "Ask a related question" at this thread titled "CCS/TMS320C6713B: Error gmake: *** [C:/Program Files (x86)/Data Translation/DT9840 Series/Examples/EXAMPLE1/DSP/Release/dt9841_6713cfg.obj] Error 1" linked under this message.
I found this problem compiling my DSK6416 project, which compiled without errors with 7.4.4 and 7.4.14 compiler installed under CCS 5.5. I've updated the compiler to version 7.4.24 and I hav found in the log:
"lab01ccfg.s62", ERROR! at line 887: [E0003] Invalid constant specification
SWI_Obj 1, KNL_swi, 0, _function, _pri, _mailbox, _arg0, _arg1, _dorta, _Order, _filter, _maxformat, _sumformat, _avgformat, _filtmaxmult, _filtsummult, _unittype
"lab01ccfg.s62", ERROR! at line 920: [E0003] Invalid constant specification
TSK_Obj 1, TSK_idle, 0, _iFXN, _iARG0, _iARG1, _iARG2, _iARG3, _iARG4, _iARG5, _iARG6, _iARG7, _iAUTOSTK, _iMANSTK, _iSTKSZ, _iSTKSEG, _iPRI, _iENV, _iEXITFLAG, _iUSETSKNAME, _iSTATREG, _Order, _filter, _maxformat, _sumformat, _avgformat, _filtmaxmult, _filtsummult, _unittype
"lab01ccfg.s62", ERROR! at line 977: [E0003] Invalid constant specification
STS_Obj 1, IDL_busyObj, 0, _prev, _filter, _maxformat, _sumformat, _avgformat, _op, _uType, _iA, _iB, _iC, _prevlow
I've downloaded all available 7.4.XX versions of CGTools and the project compiles fine with 7.4.21, 7.4.22, 7.4.23 but the compilation fails with 7.4.24
Regards,
Marcin
Related thread link: