hi ,I need to run a qt gpu application in AM3359
I've set up the environment, the details are as follows:
kernel and pvr km: build from ti-processor-sdk-linux-rt-am335x-evm-04.03.00.05 and the lcd display is well
filesystem with pvr um: use rootfs build from tisdk with configuation "processor-sdk-04.01.00.06-x11-config"
when i run my gpu app, the error message is as follows:
PVR():SGXKickTA:TA out of Mem and SPM occurred during last TA kick [0, ]
What does that mean and how can it be fixed?