Part Number: TDA4VM
Hi,
I refer the discussion at https://e2e.ti.com/support/processors/f/791/t/900935.
And run the QSGMII Ethernet Board successfully.
My config setting as,
1.Config static Ip 192.168.1.203 at ethfw
2.Config A72 ip 192.168.1.31 to ethfw static ARP.
(My PC ip is 192.168.1.120)
I can ping 192.168.1.120 on A72 linux shell.
I also can ping ethfw IP 192.168.1.203 on my PC.
But I run the ping command form My PC to A72 IP 192.168.1.31,
there is no response.
So how can I config the ethfw? Let the ping packet can be forwarded to A72.
Br, KS