Part Number: TDA4VM
Hi, expert:
From clock tree tool, the MAIN_PLL7_HSDIV0_CLKOUT is 1000MHz for superset.
But my customer is using a TDA4VM variant which C7x is supposed to run at 200MHz.
Here are my questions:
- MAIN_PLL7_HSDIV0_CLKOUT: this clock output is used by C7x and MMA, and also is input to GIC0 (which runs at 500MHz).
my question is : can we configure the MAIN_PLL7_HSDIV0_CLKOUT to 200MHz? Can GIC0 work well in the system with this configuration (maximum 200MHz) ?
- If the answer to the above question is "Yes", does SDK v7.0 support configuring C7x to other frequencies (spec via different TDA4VM variant)? and How?
please kindly share some comments.