Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3358
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3358
Hi Guarav,
Gaurav Aggarwal1 said:I am using AM3358 processor in our custom board and RTOS SDK 5 on windows host PC
I don't know what you mean by RTOS SDK 5, but I see PDK 1.0.16 is included in PRSDK 6.1.0.8.
Gaurav Aggarwal1 said:If I change update the Control Module Pad registers for the same pins in available project then it is updating the same registers.
By this I assume you mean the original flash writer project.
Gaurav Aggarwal1 said:values in Control Module Pad registers for GPMC AD(0-7), conf_gpmc_wait0 ,etc are not changing as per our custom board
Inspecting the NAND flash writer code, I see pad configuration occurs in two places:
main()
AM335X_Start()
AM335X_DEVICE_init()
AM335X_DEVICE_setPad() // FL: empty function
AM335X_NAND_open(GPMC_base_CS_0, AM335X_DEVICE_BUSWIDTH_8BIT)
PAD_ConfigMux(PAD_Conf_NANDFlash); // FL: GPMC pad config applied here
nandwriter();
The GPMC pad configuration occurs in the call to PAD_ConfigMux(). Did you modify the PAD configuration values in PAD_Conf_NANDFlash[] for your custom board? I suggest building the flash writer project in debug mode and stepping to this point in the code to see if your pad configuration settings are applied.
Regards,
Frank
Frank,
I mean RTOS SDK 5_03_00_07.
Yes you are right, I am configuring Pad values in PAD_Conf_NANDFlash[] for my custom board. But problem is that it is updating in original project not in created project by me. I copied all the source files from original files to created project and include all the header files.
Regards,
Gaurav
Hi Guarav,
Have you tried building your flash writer project in debug mode and running the code to PAD_ConfigMux() to see if your pad configuration settings are applied?
Regards,
Frank
Frank,
Yes I tried in Debug mode only but it is not updating pad configuration registers.
Regards,
Gaurav
Gaurav,
Are you positive you're building the new project correctly? Have you inspected the values in PAD_Conf_NANDFlash[] which should be written to the PAD configuration registers while stepping through PAD_ConfigMux()?
Regards,
Frank
Frank,
This problem is coming with PAD registers only. If I update other registers like GPMC registers, it is updating.
Regards,
Gaurav
Hi Guarav,
Please confirm my understanding:
static pin_muxing_t PAD_Conf_NANDFlash[] = {
{ GPMC_AD0_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD1_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD2_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD3_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD4_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD5_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD6_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_AD7_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_WAIT0_OFF, MODE(0) | PULLUP_EN| RXACTIVE},
{ GPMC_WPN_OFF, MODE(0) | RXACTIVE | PULLUP_EN},
{ GPMC_CSN0_OFF, MODE(0) | PULLUPDOWN_DISABLE},
{ GPMC_ADVN_ALE_OFF, MODE(0) | PULLUPDOWN_DISABLE},
{ GPMC_OEN_REN_OFF, MODE(0) | PULLUPDOWN_DISABLE},
{ GPMC_WEN_OFF, MODE(0) | PULLUPDOWN_DISABLE},
{ GPMC_BE0N_CLE_OFF, MODE(0) | PULLUPDOWN_DISABLE},
{ 0xFFFFFFFF },
If all of the above it true, the only thing I can conclude is there is some build problem in your new project.
Is your new project somehow picking up object files from the original project?
Regards,
Frank
Frank,
Yes your all points are valid. Let me check settings in my new project and will get back to you soon.
Can you work on https://e2e.ti.com/support/processors/f/791/t/933315. This is the first priority.
Regards,
Gaurav