This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: how to improve latency on TIDL(SSD) application?

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2

Hi experts:

I developed my application by using tidl(SSD) to detect object on image and followed the default TIDL use-case for SSD application on RTOS.

After dumping message from TDA2-evm-board, i noticed that the TDA2-evm-board was running on 27-fps but the latency was up to 173ms (average latency time from capture to display link).

Full log from TDA2-board is here:latency-log.txt

i'm wondering:

1. why does the 27-fps speed have 173 ms latency? why the latency is not 1000/27=37 ms?

2. how to improve latency down to 1000/30=33 ms?

Please comment, Thank you.

Best / regards

wxchen