Part Number: DRA829V
There are lot of properties defined in various nodes of Linux Kernel device tree files (*.dts, *.dtsi), where can I find more information about these nodes and properties.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA829V
There are lot of properties defined in various nodes of Linux Kernel device tree files (*.dts, *.dtsi), where can I find more information about these nodes and properties.
In general all the device tree documentation is captured in Linus Kernel documentation folder - Documentation/devicetree/bindings/
Below is an example on how to find the devicetree documentation file and the corresponding driver by using the compatible field of a node.
MMC node:
main_sdhci0: sdhci@4f80000 {
compatible = "ti,j721e-sdhci-8bit";
reg = <0x0 0x4f80000 0x0 0x1000>, <0x0 0x4f88000 0x0 0x400>;
interrupts = <GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 91 TI_SCI_PD_EXCLUSIVE>;
clock-names = "clk_xin", "clk_ahb";
clocks = <&k3_clks 91 1>, <&k3_clks 91 0>;
assigned-clocks = <&k3_clks 91 1>;
assigned-clock-parents = <&k3_clks 91 2>;
bus-width = <8>;
mmc-ddr-1_8v;
ti,otap-del-sel-legacy = <0x0>;
ti,otap-del-sel-mmc-hs = <0x0>;
ti,otap-del-sel-ddr52 = <0x5>;
ti,otap-del-sel-hs200 = <0x6>;
ti,otap-del-sel-hs400 = <0x0>;
ti,trm-icp = <0x8>;
ti,strobe-sel = <0x77>;
dma-coherent;
};
Identifying the devicetree documentation:
Looking for the compatible string in the Documentation folder will help in finding the documentation associated with this node.
In this example, sdhci-am654.txt file will have details of the properties used in this node.
ti-linux-kernel$ git grep "ti,j721e-sdhci-8bit" Documentation/devicetree/bindings/
Documentation/devicetree/bindings/mmc/sdhci-am654.txt: "ti,j721e-sdhci-8bit": 8 bit SDHCI on J721E device.
Documentation/devicetree/bindings/mmc/sdhci-am654.txt: ti,j721e-sdhci-8bit,
Identifying the Kernel driver associated:
Looking for the same compatible field in the driver folder will help in identifying the driver associated with the node.
In this example, sdhci_am654.c is the driver associated with this node.
ti-linux-kernel$ git grep "ti,j721e-sdhci-8bit" drivers/
drivers/mmc/host/sdhci_am654.c: .compatible = "ti,j721e-sdhci-8bit",