Other Parts Discussed in Thread: SYSBIOS
Hi,
CCSV9.3
Customer built stairstepEthernet_6678 from processors.wiki.ti.com/index.php/TMS320C6678L_Build_Configuration successfully. But the project get stuck when running and prompts:
[C66xx_0] System Analyzer Tutorial 4C QMSS successfully initialized CPPI successfully initialized PA successfully initialized EVM in StaticIP mode at 192.168.2.100 Set IP address of PC to 192.168.2.101 PASS successfully initialized Ethernet subsystem successfully initialized Ethernet eventId : 48 and vectId (Interrupt) : 7 Registration of the EMAC Successful, waiting for link up .. Network Added: If-1:192.168.2.100 ti.uia.runtime.ServiceMgr: line 88: assertion failure: A_invalidProcessCallbackFxn: Callback cannot be NULL xdc.runtime.Error.raise: terminating executionCPPI successfully initialized PA successfully initialized EVM in StaticIP mode at 192.168.2.100 Set IP address of PC to 192.168.2.101 PASS successfully initialized Ethernet subsystem successfully initialized Ethernet eventId : 48 and vectId (Interrupt) : 7 Timeout waiting for reply from PA to Pa_addMac command ti.sysbios.heaps.HeapMem: line 446: assertion failure: A_invalidFree: Invalid free xdc.runtime.Error.raise: terminating execution