Part Number: TDA4VM
I have a custom board and I want to confirm the bootmode I have set using the dip switch setting. This will provide as a sanity check for my configuration and also as the first level debug step as I am not able to boot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
I have a custom board and I want to confirm the bootmode I have set using the dip switch setting. This will provide as a sanity check for my configuration and also as the first level debug step as I am not able to boot.
The section 4.3 Boot Mode Pins of the TRM has these details. The bootmode and its configuration can be inferred by MCU_BOOTMODE and BOOTMODE.
CTRLMMR_MAIN_DEVSTAT register reflects the BOOTMODE pin values sampled at internal POR release.
CTRLMMR_WKUP_DEVSTAT register reflects the MCU_BOOTMODE pin values sampled
at internal POR release.
This FAQ mentions a python script (bootmode_util) which can be used to infer the Primary and the Secondary (backup) bootmodes and their configuration quickly.
All you need to input to the script is the CTRLMMR_MAIN_DEVSTAT and the CTRLMMR_WKUP_DEVSTAT registers. These registers can be read using either u-boot (md command), Kernel (devmem2) command, CCS (memory browser or even printing these out on the console.
python bootmode.py <CTRLMMR_WKUP_DEVSTAT in HEX> <CTRLMMR_MAIN_DEVSTAT in HEX> $ python bootmode.py --help usage: bootmode.py [-h] CTRLMMR_WKUP_DEVSTAT CTRLMMR_MAIN_DEVSTAT This scripts gives information on the bootmodes by taking the CTRLMMR_WKUP_DEVSTAT & CTRLMMR_MAIN_DEVSTAT registers as input positional arguments: CTRLMMR_WKUP_DEVSTAT Value of CTRLMMR_WKUP_DEVSTAT register in HEX CTRLMMR_MAIN_DEVSTAT Value of CTRLMMR_MAIN_DEVSTAT register in HEX optional arguments: -h, --help show this help message and exit for example: python bootmode.py 0x0 0x41
The sample output for SD boot configuration of the EVM is as below:
$ python bootmode.py 0x0 0x41 +--------------+------+ | MCU_BOOTMODE | 0x0 | +--------------+------+ | BOOTMODE | 0x41 | +--------------+------+ +-------------------+---------+ | Primary boot mode | MMC/SD | +-------------------+---------+ | Port | SD card | | Bus Width | 4bit | | FS/Raw | FS mode | +-------------------+---------+ +------------------+------+ | Backup boot mode | None | +------------------+------+ +------------------+------+
From the above output one can infer the Primary (SD) boot mode and Backup (None) and also the configuration like Port, Bus Width, FS/Raw mode etc..
All this data is picked up from the TRM data present in bootmode_TRM_data.py file.
bootmode_util: /cfs-file/__key/communityserver-discussions-components-files/791/bootmode_5F00_utils.zip
Regards,
Karan