Part Number: TDA2E
Tool/software: TI C/C++ Compiler
Hi,
Can I know all the steps to enable the early-boot late attach use-case in vision SDK Linux?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA2E
Tool/software: TI C/C++ Compiler
Hi,
Can I know all the steps to enable the early-boot late attach use-case in vision SDK Linux?
Hi,
The below steps are validated with the tda2xx platform for vision SDK 3.7 & we used ubuntu 14.04 host machine for a build
Refer the vision_sdk/docs/Linux/VisionSDK_Linux_UserGuide.pdf (Chapter 3.4: Build Linux Vision SDK for fast boot (Early boot and late attach of remote cores) ) or follow the below below steps to enable early-boot use-case.
cd ~/ /* Download the SDK */ wget https://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/03_07_00_00//exports/PROCESSOR_SDK_VISION_03_07_00_00_setuplinux.bin chmod +x PROCESSOR_SDK_VISION_03_07_00_00_setuplinux.bin /* Recommending to install the SDK in the home directory [ /~ ] */ ./PROCESSOR_SDK_VISION_03_07_00_00_setuplinux.bin
MAKECONFIG?=tda2xx_evm_linux_all # The supported config is tda2xx_evm_linux_all, tda2px_evm_linux_all, tda2ex_evm_linux_all, etc
Add the below changes in vision_sdk/apps/configs/$MAKECONFIG/cfg.mk file
EARLY_USECASE_ENABLE=yes
sudo apt-get install -y ssh corkscrew gawk sed u-boot-tools dos2unix dtrx git lib32z1 lib32ncurses5 lib32bz2-1.0 libc6-i386 libc6:i386 libstdc++6:i386 libncurses5:i386 libz1:i386 libc6-dev-i386 device-tree-compiler mono-complete lzop
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/ti_components/os_tools/linux/linaro/ wget https://releases.linaro.org/components/toolchain/binaries/5.3-2016.02/arm-linux-gnueabihf/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf.tar.xz tar -xvf gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf.tar.xz
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/build/ ./hlos/scripts/linux/setup_linux.sh
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/ti_components/os_tools/linux/targetfs/ chmod 777 ../targetfs/ wget https://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/03_07_00_00//exports/tisdk-rootfs-image-dra7xx-evm_vsdk_3_7.tar.xz --no-check-certificate tar xf tisdk-rootfs-image-dra7xx-evm_vsdk_3_7.tar.xz rm tisdk-rootfs-image-dra7xx-evm_vsdk_3_7.tar.xz
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/ti_components/os_tools/linux/kernel/omap/ /* The below one command is needed only for the VSDK 3.7 SDK to reset the Git commit */ git reset --hard 9e4a96e876ff8cfffe8694f38f27635dfbc18f3f git am ../linux-kernel-addon/earlyboot-kernel-patches/*
/* Here the Early use-case is defined */ ~/PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/apps/src/rtos/usecases/early_capture_late_weston
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/build/ make linux make linux_install make -s -j depend make -s -j
cd ~/PROCESSOR_SDK_VISION_03_07_00_00/ti_components/os_tools/linux/targetfs/ tar cvf tisdk-rootfs-image-dra7xx-evm.tar.xz ./* mv tisdk-rootfs-image-dra7xx-evm.tar.xz ~/PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/binaries/apps/tda2xx_evm_linux_all/hlos/linux/boot/ cd ~/PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/build/ sudo ./hlos/scripts/linux/mksdboot.sh --device /dev/<parent_device_name> --appname <MAKEAPPNAME> --makeconfig <MAKECONFIG> # ex: sudo ./hlos/scripts/linux/mksdboot.sh --device /dev/sdc --appname apps --makeconfig tda2xx_evm_linux_all
./hlos/scripts/linux/early-boot-update.sh <makeconfig> <path to target FS> <path to boot-partition> # Ex: ./hlos/scripts/linux/early-boot-update.sh tda2xx_evm_linux_all ~/PROCESSOR_SDK_VISION_03_07_00_00/ti_components/os_tools/linux/targetfs /media/gaviraju/boot
reading single-stage-boot.dtb reading uImage reading uImage [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 4.4.84+ (x1046101local@udx1046101) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #2 SMP PREEMPT Thu Jul 16 18:33:30 IST 2020 [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] Machine model: TI DRA742 [ 0.000000] bootconsole [earlycon0] enabled
cd /opt/vision_sdk/ ./vision_sdk_load.sh ./apps.out
[HOST] [IPU2 ] 1.576459 s: DISPLAY: Create in progress !!! [HOST] [IPU2 ] 1.577099 s: DISPLAY: Create Done !!! [HOST] [IPU2 ] 1.675983 s: DISPLAY: Start in progress !!! [HOST] [IPU2 ] 1.676075 s: DISPLAY: Start Done !!!
Thanks
Gaviraju