Part Number: TDA4VM
Hi
■Problem
DMVD instruction of c6x is not emulated correctly.
A build error occurs.
Checked on both Host Emulation and actual c7x.
■Test code
■Result
■Reference
TMS320C6000 Optimizing Compiler v 7.4 User's Guide (Rev. U) P.220
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi
■Problem
DMVD instruction of c6x is not emulated correctly.
A build error occurs.
Checked on both Host Emulation and actual c7x.
■Test code
■Result
■Reference
TMS320C6000 Optimizing Compiler v 7.4 User's Guide (Rev. U) P.220
The root cause is an error in the C6000 compiler manual. In the description of the _dmvd intrinsic, the type of the first argument is incorrectly shown as long long. It should be unsigned. The correct interface is ...
long long _dmvd(unsigned src1, unsigned src2);
In your simple test case the invocation of _dmvd should be changed to: int64_t llResult = _dmvd(0, 0);
I filed EXT_EP-10242 to have the C6000 compiler manual corrected. You are welcome to follow it with that link.
Thanks and regards,
-George