Hello,
We have designed a simple 4 touch board using MSP430FR2512, using CAP0.0, CAP0.1, CAP0.2, and CAP0.3 in self capacitance mode with no proximity sensing. Currently, all noise immunity has been enabled in the config file as shown below:
However, during EFT Clamp Testing at 2000V, 100kHz, the noise in the buttons is causing the capacitive touch buttons to have pushes when no one is pushing the buttons.
Kindly help us on this at the earliest as we seek immediate help on this.