Part Number: TDA4VM
Hi
I'm facing the trouble at "TVM/Neo-AI-DLR + TIDL Heterogeneous Execution".
I' m referring at the "TIDL specific lines in compilation script" in
software-dl.ti.com/.../md_tidl_osr_tvm_tidl.html
and also referring "est_tidl_j7.py".
The problem is that I cannot compile the Pytorch model directly (i.e. without Onnx) for EVM.
But, it's ended with error as below.
It's happened only when I try to compile with a large number of images (up to 100) used for quantization calibration.
The model I use is same with one on e2e.ti.com/.../977560.
Thanks and Best regards,
HaTa