Other Parts Discussed in Thread: TMS320C6745
Hi
I have some problems and doubts with the hardware of the target that i`m doing for the TMS320C6745 (TMX320C6745PTP3 , 176-pin TQFP). In the JTAG configuration of the Emulator XDS510USB PLUS, there are two pins: EMU0 and EMU1 that must be connected with the pins EMU0 and EMU1 of the DSP, the problem is that the C6745 doesn´t have this pins, so, what do i do with this pins?
What oscilator frequency do i have to use with the C6745? (I already have a 24MHz oscilator with 2 capacitors of 18pF)
Is the /reset pin(146) necessary to programm the dsp?
What is the core power supply (CVDD) for? It is necessary for the programming?
What is the minimum hardware that i need to programm the dsp (Jtag pins, oscilator?, VDD)?
Thanks in advance
LauRa