Hello,
I have a 32K block of NVRAM hanging on the GPMC at CS1. When I tried to access this memory space, I can only go up to 4K Bytes. Address GPMC_A11 to GPMC_A14 stay at 0 and never go high. For experiment, I reconfigured the GPMC_A11-GPMC_A14 as GPIO and set them high. I was able to see the memory above 4K after I set these lines high, so I know that these lines are not stuck low. The TI816X spec stated that the minimum range for GPMC CS is 16M Bytes, so I should have ample of room for my 32K Bytes memory.
The mux pins at AC2, H2, H6, H5 are configured for GPMC_A11-GPMC_A14 respectively. It seems the chip thinks that I only have 4K Bytes of memory. What could be causing this problem?
Thanks,
Tri