Hello,
I'm trying to setup a link for EDMA to McASP on the C6748. OPT0 is used for the initial McASP Rx and OPT1 for Tx. The user guide says to link the initial PARAM that to another PARAM, which is linked back to itself. So I've used an offset of 2, i.e. OPT0 will link to OPT2, which will link back to itself. OPT1 will link to OPT3. So for Rx:
OPT0.LINK_BCNTRLD0 = 0x4060 // link to OPT2
OPT2. LINK_BCNTRLD2 = 0x4060 // link to itself
Is there a reason not to just stick with OPT0, and have the link back to itself, instead of to OPT2? The user guide seemed to imply that OPT0 is just for the initial DMA, and the another OPT (2 in my case) is needed for all subsequent.
Please advise,
Robert