Hi, everyone:
I use the C6678 for jpeg encoder, the jpeg encoder codec version is C66x_jpegenc_02_02_00_01_ELF.
My question is when I encode the picture without the DRI Marker, the encode total time is about 80ms, while with the DRI Marker, the total time is about 300ms!!! When I change the DRI_Interval, it is also about 300ms!!!
Is it ture? (I am sure that the encoded jpeg picture is right, and the size of the picture with or without DRI Marker is almost the same.)
thanks a lot.