This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Image Processing Example

Hello, I was trying to implement the Image Processing Example on my 6678 board.

but unfortunately it didn't work. I connect my board to a hub which my PC connect as well. 

the print-off infos from the console are shown as below: 

[C66xx_0] MessageQ_open MultiCoreTypes_MASTERSTARTED


MCSDK IMAGE PROCESSING DEMONSTRATION

QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
EVM in StaticIP mode at 192.168.2.100
Set IP address of PC to 192.168.2.101
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
Service Status: HTTP : Enabled : : 000
Setting IpcMP_module->replyMQ 0x3, 0x30000
Setting IpcMP_module->replyMQ 0x1, 0x10000
Setting IpcMP_module->replyMQ 0x4, 0x40000
Setting IpcMP_module->replyMQ 0x5, 0x50000
Setting IpcMP_module->replyMQ 0x6, 0x60000
Setting IpcMP_module->replyMQ 0x7, 0x70000
Setting IpcMP_module->replyMQ 0x2, 0x20000

ps: I'm using CCSv5.4

      XDCtools version : 3.23.4.60

      IMGLIB: 3.1.1.0

      IPC: 1.24.3.32

      MCSDK: 2.1.2.6

      NDK: 2.21.2.43

      SYS/BIOS: 6.35.1.29

      Generation Tool version: 7.4.2

before I load .out seperately to all the cores, I resetted my system, and load GEL file for each core and did the global initialization. 

Hope to get some responses.

Best regards,

Wendy