hello,
i m trying to use the LAN8710A for a customer board based on AM335x with RMII mode.
1-) clock 50MHZ sourced from AM335x :
==> when trying to ping the board on network 100Mb, i get near of 40% packet loss.
==> when trying to ping the board on network 10Mb, no packet loss
2-) clock 50MHz sourced from external oscillator:
==> can't get the LAN8710A work: i made changes on gmii_sel register (rmii1_io_clk_en bit) but with no results. did i miss somethings on configuration ?
the Pinmux is configured as RMII mode,
thanks