This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X u-boot boot kernel problem



Hi, everyone

   My study board is AM335x SK board,  BSP version is SDK7.0

  SDK7.0, the kernel & DTB on the second partition,  I want to put the kernel & DTB on the first partition

  I don't know that u-boot modify the code?

  • Hi Ryan,

    I have forwarded this to the SW people.

  • Did you solve it?

  • Hi, I have a similar board and another problem with the u-boot-Bootmanager ...:
    I've a BBB (BeagleBone Black) with an AM335x...
    I try to boot different kernels using U-Boot, TFTP, ... over network - an I get strange results I can't understand what's happening... Instead of booting the kernel I see annoying reboots all the time (with different Kernel-Images!?!) - here an example:

    The first rows are working fine (setting all the parameters in the u-boot-terminal ..., loading the images via network, ...) but then instead of loading the Kernel it crashes...
    ------------------------
    U-Boot# setenv serverip 10.123.200.10
    U-Boot# setenv ipaddr 10.123.200.12
    U-Boot# setenv fdt_high ffffffff; saveenv
    Saving Environment to NAND...
    Erasing NAND...
    Attempt to erase non block-aligned data
    U-Boot# setenv kernel_addr 0x80008000
    U-Boot# setenv fdt_addr 0x80f80000
    U-Boot# tftpboot ${kernel_addr} uImage-new
    link up on port 0, speed 100, full duplex
    Using cpsw device
    TFTP from server 10.123.200.10; our IP address is 10.123.200.12
    Filename 'uImage-new'.
    Load address: 0x80008000
    Loading: *#################################################################
    #################################################################
    #################################################################
    #################################################################
    ###################################################
    1.6 MiB/s
    done
    Bytes transferred = 4560377 (4595f9 hex)
    U-Boot# tftpboot ${fdt_addr} am335x-bb.dtb
    link up on port 0, speed 100, full duplex
    Using cpsw device
    TFTP from server 10.123.200.10; our IP address is 10.123.200.12
    Filename 'am335x-bb.dtb'.
    Load address: 0x80f80000
    Loading: *##
    1.7 MiB/s
    done
    Bytes transferred = 23769 (5cd9 hex)
    U-Boot# setenv bootargs console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
    U-Boot# bootm ${kernel_addr} - ${fdt_addr}
    ## Booting kernel from Legacy Image at 80008000 ...
    Image Name: Linux-3.8.13-rt9-00899-gd04fb13
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 4560313 Bytes = 4.3 MiB
    Load Address: 80008000
    Entry Point: 80008000
    Verifying Checksum ... OK
    ## Flattened Device Tree blob at 80f80000
    Booting using the fdt blob at 0x80f80000
    XIP Kernel Image ... OK
    Using Device Tree in place at 80f80000, end 80f88cd8

    Starting kernel ...

    data abort
    pc : [<8000800c>] lr : [<9f74c214>]
    sp : 9f62ac90 ip : ffffffff fp : 9f7a34ec
    r10: 00000000 r9 : 9f62af28 r8 : 9f6313a4
    r7 : 00000000 r6 : 80008000 r5 : 9f7a7374 r4 : 00000000
    r3 : 00005cd9 r2 : 80f80000 r1 : 00000e05 r0 : 9f62afe0
    Flags: nZCv IRQs off FIQs on Mode SVC_32
    Resetting CPU ...

    resetting ...

    U-Boot SPL 2014.04-00014-g47880f5 (Apr 22 2014 - 13:23:54)
    reading args
    spl_load_image_fat_os: error reading image args, err - -1
    reading u-boot.img
    reading u-boot.img
    --------------------------
    Does someone knew the problem, has any good informations, a link to an example, ...?!?
    Thank's very much!
  • hi,
    I only try under command line, file store SD Card
    go to u-boot stop, the step:
    1. fatload mmc 0:1 ${loadaddr} zImage
    2. fatload mmc 0:1 ${fdtaddr} am335x-evmsk.dtb
    3. run mmcargs
    4. bootz ${loadaddr} - ${fdtaddr}
  • Thanks!
    A good idea to try it with the SD-Card!
    Another good link I got in another thread is that one:
    http://elinux.org/Building_BBB_Kernel#Transferring_the_image_to_the_BBB_via_TFTP