Other Parts Discussed in Thread: TMS320C5515
Hi,
Im using C5515 DSP with 24-bit SPI flash for application code.I do not have any other memory interface other than 64mb mSDRAM.
The document "Using the TMS320C5515/14/05/04 Bootloader - SPRABD7C" mentions that the 24-bit SPI flash doesn't support boot image encryption but the TMS320C5515/14 Silicon Revision 2.0 Silicon errata mentions only the Encrypted reauthoring and Bound to device mode is not supported for 24-bits SPI. Even though the Silicon errata holds precedence over SPRABD7C Doc, I want to conform whether the 24-bit SPI flash supports encrypted boot with device bound mode.
Has anyone tried to encrypting boot image on 24-bit SPI flash and been successful?
Regards
SK