This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Camera CSI2. Do I need to enable ISP?

Hi. Working on a camera with CSI2. So far I'm focusing on the imaging subsystem (ISS). I know that the image signal processor ISP is a sub-component to the ISS. It looks like the ISP can do some fancy things, that I probably don't need. At this time I keep the ISP disabled. Is that a bad idea and do I need to work with the ISP as well? All I want to do is take still images and I'm not (yet) worried about white balance and all that stuff.

Also is it ok to post here if I am using the OMAP4430? It looked like the appropriate forum is read-only.