Tool/software: TI-RTOS
We are trying to capture an picture image using balser camera which output Discrete YUV422 signal,for this purpose we chose DM8148 processor using mjeg alg encode type.
However, the image was like :
- fact1:
the link chain :captureLink -> encLink(mJpeg)-> A8host
We use SYSTEM_STD_720P_60 as default pixs 1280 * 720, the green on both sides exists.
We tried to change SYSTEM_STD_720P_60 in bios6 firmware as 1024 * 720 pixs, while the green on both sides stil exists, we try to belieive that there is something wrong with mjeg encode link
- fact2
Link chain: captureLink -> enclink(h264) ->A8host
The video h264 file looks just the same as mjeg picture, what ???!!! , does it mean the encode link is just fine and the problem comes with captureLink?
- question
For the moment we need to dignify what causes the problem, enclink? if not , how to configure captureLink in bios6 as we need the correct discrete time sequence, any answers would be of great help, thanks.
- picture
this image is 1280 *720pixs in jpg format , the green color is a little weired, the 1024 * 720 pixs in jpg format image and the h264 video file as well