This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

time test



I  am using the fuction  clock() to test the  program running time  in CCS 3.3

But the time tested by the function clock() is different the time tested  manually  with my mobilephone.

For example ,a program time tested by clock() is  160ms ,and when I run the program for 100 times,the time tested is near 160ms*100=16s.

But the time tested manually is more than 80 s.

furthernore ,the cpu clock is set to 600MHz.   In the program the CLOCKS_PER_SEC is set to 200MHz.

So I expect the time tested manually is 16/3s=5s rather than 80s.