Hi,
I'm using the C5515 ezdsp and the CSL USB-DMA example. I've found that enumeration does not occur if I run the example without having USB0 connected in advance. I've found some piece of code in this forum to solve this problem. However, I still have the problem that re-enumeration does not happen if I disconnect the cable and then re-connect it. What do I have to add to the code (I guess in usb_isr function)?
Thank you very much for your answers.
Best regards,
Andreas