Other Parts Discussed in Thread: OMAPL138
Hello,
We are using LCDKC6748 module and "pdk_omapl138_1_0_3" sdk. and we are using TIRTOS. Our application is Data logging.
When I use the "USB_HostMsc_lcdkOMAPL138_c674xExampleProject" to store data in 16 GB pendrive. The example is working fine.
When I modify the program to store the data which I aquire in a Timer function which runs at10ms I get FR_DISK_ERR while using f_write funciton. I am trying to write only 10bytes to the file in the timer function very frequently I am getting FR_DISK_ERR error. We I check the byteswritten variable during this error it was less than 10 bytes.
Kindly suggest me how to solve this problem
Thanks & regards
Navaneetha krishnan