This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TCI6638K2K: Boot issue after changing NAND

Part Number: TCI6638K2K


Tool/software: Linux

Hi,

We have changed the NAND flash in our custom board, which is having different part number and size.

Part number is: Cypress S34MS16G202BHI000

Nand size: 2GiB

Input / Output Bus Width: 8-bits
Page Size: (2048 + 128) bytes; 128-byte spare area
Block Size: 64 Pages or (128k + 8k) bytes
Plane Size: 2048 Blocks per Plane or (256M + 16M) bytes
Device Size: 2 Planes per Device or 512 Mbyte

We created the ubifs image with following commands,

./mkfs.ubifs -r tisdk-rootfs-rt-k2hk-evm/ -o k2k_rootfs.ubifs.img -F -m 2048 -e 126976 -c 16100
./mkfs.ubifs -r boot/ -o k2k_boot.ubifs.img -F -m 2048 -e 126976 -c 99

vi ubinize.cfg

[boot]
mode=ubi
image=k2k-boot.ubifs.img
vol_type=dynamic
vol_id=0
vol_name=boot
vol_size=10MiB
[rootfs]
mode=ubi
image=k2k_rootfs.ubifs.img
vol_id=1
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize

./ubinize -o k2k_BBM.ubi -m 2048 -p 128KiB -s 2048 -O 2048 ubinize.cfg

bootarg variable as:

setenv args_ubi 'setenv bootargs ${bootargs} rootfstype=ubifs root=ubi1:rootfs rootflags=sync rw ubi.mtd=2,2048'

boot log as follows:

U-Boot 2013.01 (Jun 07 2019 - 17:41:06)

I2C:   ready
DDR3 speed 1600

Reseting entire DDR3 memory to 0 ...
DRAM:  2 GiB
NAND:  pagesize 0
writesize 2048
erasesize 131072
oobsize 128
busw 0
2048 MiB
Net:   K2HK_EMAC
Warning: K2HK_EMAC using MAC address from net device
, K2HK_EMAC1, K2HK_EMAC2, K2HK_EMAC3
Hit any key to stop autoboot:  0
Creating 1 MTD partitions on "nand0":
0x000000180000-0x000080000000 : "mtd=2"
UBI: attaching mtd1 to ubi0
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
UBI: volume 1 ("rootfs") re-sized from 3440 to 16117 LEBs
UBI: attached mtd1 to ubi0
UBI: MTD device name:            "mtd=2"
UBI: MTD device size:            2046 MiB
UBI: number of good PEBs:        16367
UBI: number of bad PEBs:         5
UBI: max. allowed volumes:       128
UBI: wear-leveling threshold:    4096
UBI: number of internal volumes: 1
UBI: number of user volumes:     2
UBI: available PEBs:             0
UBI: total number of reserved PEBs: 16367
UBI: number of PEBs reserved for bad PEB handling: 163
UBI: max/mean erase counter: 1/0
UBIFS: mounted UBI device 0, volume 0, name "boot"
UBIFS: mounted read-only
UBIFS: file system size:   9269248 bytes (9052 KiB, 8 MiB, 73 LEBs)
UBIFS: journal size:       1904640 bytes (1860 KiB, 1 MiB, 15 LEBs)
UBIFS: media format:       w4/r0 (latest is w4/r0)
UBIFS: default compressor: LZO
UBIFS: reserved for root:  0 bytes (0 KiB)
Loading file 'securedb.key.bin' to addr 0x0c000000 with size 28 (0x0000001c)...
Done
Loading file 'uImage-k2hk-evm.dtb' to addr 0x87000000 with size 54332 (0x0000d43c)...
Done
Loading file 'skern-k2hk-evm.bin' to addr 0x0c5f0000 with size 45056 (0x0000b000)...
Done
Loading file 'uImage-keystone-evm.bin' to addr 0x88000000 with size 4158720 (0x003f7500)...
Done
## installed monitor, freq [200000000], status 0
## Booting kernel from Legacy Image at 88000000 ...
   Image Name:   Linux-3.10.72-rt77_BBM_V1.0.0
   Created:      2019-06-12   7:17:15 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4158656 Bytes = 4 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 87000000
   Booting using the fdt blob at 0x87000000
   Loading Kernel Image ... OK
OK
   Using Device Tree in place at 87000000, end 8701043b

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 3.10.72-rt77_BBM_V1.0.0 (yash@yash) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.039
[    0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c7387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] Machine: KeyStone2, model: Texas Instruments Keystone 2 SoC
[    0.000000] switching to high address space at 0x800000000
[    0.000000] cma: CMA: reserved 16 MiB at 2e800000
[    0.000000] Memory policy: ECC enabled, Data cache writealloc
[    0.000000] PERCPU: Embedded 9 pages/cpu @c1066000 s12480 r8192 d16192 u36864
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260624
[    0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 rootfstype=ubifs root=ubi0:rootfs rootflags=sync rw ubi.mtd=2,2048
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 1024MB = 1024MB total
[    0.000000] Memory: 1013844k/1013844k available, 34732k reserved, 270336K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc074be28   (7440 kB)
[    0.000000]       .init : 0xc074c000 - 0xc079a0c0   ( 313 kB)
[    0.000000]       .data : 0xc079c000 - 0xc0802c18   ( 412 kB)
[    0.000000]        .bss : 0xc0802c18 - 0xc083e2d4   ( 238 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] ipc irq: irqchip registered, range 512-539
[    0.000000] Main PLL clk (1200000000 Hz), parent (122880000 Hz),postdiv = 2, mult = 624, prediv = 31
[    0.000000] Generic PLL clk (1400000000 Hz), parent (125000000 Hz),postdiv = 1, mult = 55, prediv = 4
[    0.000000] Generic PLL clk (1228800000 Hz), parent (122880000 Hz),postdiv = 2, mult = 19, prediv = 0
[    0.000000] Generic PLL clk (400000000 Hz), parent (100000000 Hz),postdiv = 4, mult = 15, prediv = 0
[    0.000000] Generic PLL clk (400000000 Hz), parent (100000000 Hz),postdiv = 4, mult = 15, prediv = 0
[    0.000000] Architected local timer running at 200.00MHz (phys).
[    0.000000] Switching to timer-based delay loop
[    0.000000] sched_clock: ARM arch timer >56 bits at 200000kHz, resolution 640/128ns
[    0.000000] keystone timer clock @200000000 MHz
[    0.000000] sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms
[    0.000000] Console: colour dummy device 80x30
[   72.669469] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=2000000)
[   72.669471] pid_max: default: 4096 minimum: 301
[   72.669581] Mount-cache hash table entries: 512
[   72.677942] CPU: Testing write buffer coherency: ok
[   72.678091] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[   72.678107] psci: probing function IDs from device-tree
[   72.678120] Setting up static identity map for 0xc0524fa0 - 0xc0524ff8
[   72.793779] CPU1: Booted secondary processor
[   72.793804] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[   72.833819] CPU2: Booted secondary processor
[   72.833844] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[   72.873837] CPU3: Booted secondary processor
[   72.873862] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[   72.873978] Brought up 4 CPUs
[   72.873996] SMP: Total of 4 processors activated (1600.00 BogoMIPS).
[   72.874000] CPU: All CPU(s) started in SVC mode.
[   72.874424] devtmpfs: initialized
[   72.888149] NET: Registered protocol family 16
[   72.889563] DMA: preallocated 256 KiB pool for atomic coherent allocations
[   72.903895] No ATAGs?
[   72.903911] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[   72.903917] hw-breakpoint: maximum watchpoint size is 8 bytes.
[   72.914997] bio: create slab <bio-0> at 0
[   72.915415] keystone-pcie: keystone_pcie_rc_init - start
[   72.915437] keystone2_pcie_serdes_setup for domain 0
[   72.917557] keystone2_pcie_serdes_setup done domain 0, en_link_train = 1
[   72.917585] keystone-pcie: MEM 0x0000000050000000..0x000000005fffffff -> 0x0000000050000000
[   72.917594] keystone-pcie: IO 0x0000000023250000..0x0000000023253fff -> 0x0000000000000000
[   72.917625] keystone-pcie: pcie - number of legacy irqs = 4
[   72.917668] keystone-pcie: pcie - number of MSI host irqs = 8, msi_irqs = 32
[   73.019487] keystone-pcie: Doing PCI Setup...Done
[   73.019492] keystone-pcie: Starting PCI scan, nr 0...
[   73.019622] PCI host bridge to bus 0000:00
[   73.019632] pci_bus 0000:00: root bus resource [mem 0x50000000-0x5fffffff]
[   73.019639] pci_bus 0000:00: root bus resource [io  0x0000-0x3fff]
[   73.019645] pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
[   73.019678] PCI: bus0: Fast back to back transfers enabled
[   73.019694] keystone-pcie: Ending PCI scan...
[   73.019702] keystone-pcie: keystone_pcie_rc_init - end
[   73.019991] vgaarb: loaded
[   73.020322] SCSI subsystem initialized
[   73.020952] usbcore: registered new interface driver usbfs
[   73.021041] usbcore: registered new interface driver hub
[   73.021144] usbcore: registered new device driver usb
[   73.022648] pps_core: LinuxPPS API ver. 1 registered
[   73.022653] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[   73.022723] PTP clock support registered
[   73.022844] keystone-hwqueue hwqueue.8: qmgr start queue 0, number of queues 8192
[   73.022919] keystone-hwqueue hwqueue.8: added qmgr start queue 0, num of queues 8192, reg_peek f0040000, reg_status f0006000, reg_config f00080
[   73.022928] keystone-hwqueue hwqueue.8: qmgr start queue 8192, number of queues 8192
[   73.022998] keystone-hwqueue hwqueue.8: added qmgr start queue 8192, num of queues 8192, reg_peek f0100000, reg_status f000c400, reg_config f00
[   73.023627] keystone-hwqueue hwqueue.8: qos: sched port @8096, drop sched @8000
[   73.024118] keystone-hwqueue hwqueue.8: qos: sched port @6496, drop sched @6400
[   73.024927] keystone-hwqueue hwqueue.8: added pool pool-rio: 128 descriptors of size 256
[   73.024936] keystone-hwqueue hwqueue.8: added pool pool-xge: 1024 descriptors of size 128
[   73.024945] keystone-hwqueue hwqueue.8: added pool pool-crypto: 1024 descriptors of size 128
[   73.024953] keystone-hwqueue hwqueue.8: added pool pool-net: 11264 descriptors of size 128
[   73.024960] keystone-hwqueue hwqueue.8: added pool pool-udma: 1920 descriptors of size 256
[   73.027808] keystone-hwqueue hwqueue.8: registered queues 0-16383
[   73.028086] keystone-hwqueue hwqueue.8: qos version 0x200010b, magic valid
[   73.028571] keystone-hwqueue hwqueue.8: qos version 0x200010b, magic valid
[   73.035820] keystone-pktdma 2a08000.pktdma: registered 32 logical channels, flows 32, tx chans: 32, rx chans: 32, loopback
[   73.039681] keystone-pktdma 2004000.pktdma: registered 33 logical channels, flows 32, tx chans: 9, rx chans: 24
[   73.040229] keystone-pktdma 2fa1000.pktdma: registered 4 logical channels, flows 32, tx chans: 16, rx chans: 16
[   73.040399] Switching to clocksource arch_sys_counter
[   73.062638] NET: Registered protocol family 2
[   73.063117] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[   73.063231] TCP bind hash table entries: 8192 (order: 5, 229376 bytes)
[   73.063445] TCP: Hash tables configured (established 8192 bind 8192)
[   73.063487] TCP: reno registered
[   73.063496] UDP hash table entries: 512 (order: 3, 32768 bytes)
[   73.063534] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[   73.063739] NET: Registered protocol family 1
[   73.063922] RPC: Registered named UNIX socket transport module.
[   73.063927] RPC: Registered udp transport module.
[   73.063932] RPC: Registered tcp transport module.
[   73.063936] RPC: Registered tcp NFSv4.1 backchannel transport module.
[   73.064281] hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
[   73.118979] bounce pool size: 64 pages
[   73.127248] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[   73.127319] NTFS driver 2.1.30 [Flags: R/O].
[   73.127566] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[   73.127906] msgmni has been set to 1484
[   73.128787] NET: Registered protocol family 38
[   73.128993] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
[   73.129000] io scheduler noop registered
[   73.129005] io scheduler deadline registered
[   73.129241] io scheduler cfq registered (default)
[   73.130840] keystone-udma udma0.9: registered udma device udma0
[   73.190784] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[   73.192392] 2530c00.serial: ttyS0 at MMIO 0x2530c00 (irq = 309) is a 16550A
[   74.039871] console [ttyS0] enabled
[   74.044066] 2531000.serial: ttyS1 at MMIO 0x2531000 (irq = 312) is a 16550A
[   74.054653] loop: module loaded
[   74.057933] at24 0-0050: 131072 byte 24c1024 EEPROM, writable, 1 bytes/write
[   74.066498] Generic platform RAM MTD, (c) 2004 Simtec Electronics
[   74.073499] ONFI param page 0 valid
[   74.076996] erasesize 131072
[   74.079880] writesize 2048
[   74.082590] oobsize 128
[   74.085038] busw 0
[   74.087050] ONFI flash detected
[   74.090200] NAND device: Manufacturer ID: 0x01, Chip ID: 0xa5 (AMD/Spansion S34MS16G2), 2048MiB, page size: 2048, OOB size: 128
[   74.101717] 'erasesize 131072
[   74.104689] writesize 2048
[   74.107397] oobsize 128
[   74.109844] busw 0
[   74.111857] chunks 4
[   74.114317] Bad block table found at page 1048512, version 0x02
[   74.120721] Bad block table found at page 1048448, version 0x02
[   74.127133] nand_read_bbt: bad block at 0x000031440000
[   74.132388] 3 ofpart partitions found on MTD device 30000000.nand
[   74.138500] Creating 3 MTD partitions on "30000000.nand":
[   74.143917] 0x000000000000-0x000000100000 : "u-boot"
[   74.149637] 0x000000100000-0x000000180000 : "params"
[   74.155306] 0x000000180000-0x000040000000 : "ubifs"
[   74.161199] davinci_nand 30000000.nand: controller rev. 2.5
[   74.167449] spi_davinci 21000400.spi: master is unqueued, this is deprecated
[   74.174791] m25p80 spi32766.0: found n25q128a11, expected n25q128
[   74.180907] m25p80 spi32766.0: n25q128a11 (16384 Kbytes)
[   74.186243] 2 ofpart partitions found on MTD device spi32766.0
[   74.192094] Creating 2 MTD partitions on "spi32766.0":
[   74.197248] 0x000000000000-0x000000080000 : "u-boot-spl"
[   74.203248] 0x000000080000-0x000001000000 : "test"
[   74.209049] spi_davinci 21000400.spi: Controller at 0xf007a400
[   74.215215] spi_davinci 21000600.spi: master is unqueued, this is deprecated
[   74.222626] spi_davinci 21000600.spi: Controller at 0xf007c600
[   74.228780] spi_davinci 21000800.spi: master is unqueued, this is deprecated
[   74.235855] spi_davinci 21000800.spi: Controller at 0xf007e800
[   74.242878] tun: Universal TUN/TAP device driver, 1.6
[   74.247945] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[   74.254693] keystone-netcp 2090000.netcp: number of serdeses 1
[   74.260559] keystone-netcp 2090000.netcp: Missing cpts_clock_mult property in the DT.
[   74.268416] keystone-netcp 2090000.netcp: Missing cpts_clock_shift property in the DT.
[   74.276361] keystone-netcp 2090000.netcp: Missing cpts_clock_div property in the DT.
[   74.285070] keystone-netcp 2090000.netcp: cpsw serdes 0 config done lanes(mask) 0xf
[   74.293644] keystone-netcp 2090000.netcp: Created interface "eth0"
[   74.299850] keystone-netcp 2090000.netcp: dma_chan_name nettx0
[   74.306582] keystone-netcp 2090000.netcp: Created interface "eth1"
[   74.312788] keystone-netcp 2090000.netcp: dma_chan_name nettx1
[   74.319488] keystone-netcp 2090000.netcp: Created interface "eth2"
[   74.325695] keystone-netcp 2090000.netcp: dma_chan_name nettx2
[   74.332411] keystone-netcp 2090000.netcp: Created interface "eth3"
[   74.338616] keystone-netcp 2090000.netcp: dma_chan_name nettx3
[   74.344601] keystone-netcp 2090000.netcp: pdsp 0 firmware: keystone/pa_pdsp0_classify1.fw
[   74.352809] keystone-netcp 2090000.netcp: pdsp 1 firmware: keystone/pa_pdsp1_classify1.fw
[   74.361018] keystone-netcp 2090000.netcp: pdsp 2 firmware: keystone/pa_pdsp2_classify1.fw
[   74.369226] keystone-netcp 2090000.netcp: pdsp 3 firmware: keystone/pa_pdsp3_classify2.fw
[   74.377433] keystone-netcp 2090000.netcp: pdsp 4 firmware: keystone/pa_pdsp45_pam.fw
[   74.385205] keystone-netcp 2090000.netcp: pdsp 5 firmware: keystone/pa_pdsp45_pam.fw
[   74.393158] keystone-netcp 2090000.netcp: could not find interface 2 node in device tree
[   74.401279] keystone-netcp 2090000.netcp: Attach of module keystone-qos declined with -19
[   74.409487] keystone-netcp 2090000.netcp: could not find interface 3 node in device tree
[   74.417607] keystone-netcp 2090000.netcp: Attach of module keystone-qos declined with -19
[   74.425830] keystone-netcp 2090000.netcp: Attach of module keystone-sa declined with -19
[   74.433950] keystone-netcp 2090000.netcp: Attach of module keystone-sa declined with -19
[   74.443162] dwc3 2690000.dwc3: no usb2 phy configured
[   74.448238] platform 2690000.dwc3: Driver dwc3 requests probe deferral
[   74.455293] usbcore: registered new interface driver usb-storage
[   74.461783] mousedev: PS/2 mouse device common for all mice
[   74.467598] i2c /dev entries driver
[   74.471763] watchdog 22f0080.wdt: heartbeat 60 sec
[   74.487755] keystone-crypto 20c0000.crypto: crypto accelerator enabled
[   74.494679] usbcore: registered new interface driver usbhid
[   74.500269] usbhid: USB HID core driver
[   74.504464]  remoteproc0: 2620040.dsp0 is available
[   74.509356]  remoteproc0: Note: remoteproc is still under development and considered experimental.
[   74.518345]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.528760]  remoteproc0: no firmware found
[   74.533086] rproc-user 2620040.dsp0: registered misc device dsp0
[   74.539376]  remoteproc1: 2620044.dsp1 is available
[   74.544268]  remoteproc1: Note: remoteproc is still under development and considered experimental.
[   74.553259]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.563675]  remoteproc1: no firmware found
[   74.567994] rproc-user 2620044.dsp1: registered misc device dsp1
[   74.574287]  remoteproc2: 2620048.dsp2 is available
[   74.579178]  remoteproc2: Note: remoteproc is still under development and considered experimental.
[   74.588168]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.598580]  remoteproc2: no firmware found
[   74.602897] rproc-user 2620048.dsp2: registered misc device dsp2
[   74.609180]  remoteproc3: 262004c.dsp3 is available
[   74.614073]  remoteproc3: Note: remoteproc is still under development and considered experimental.
[   74.623064]  remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.633475]  remoteproc3: no firmware found
[   74.637798] rproc-user 262004c.dsp3: registered misc device dsp3
[   74.644084]  remoteproc4: 2620050.dsp4 is available
[   74.648975]  remoteproc4: Note: remoteproc is still under development and considered experimental.
[   74.657965]  remoteproc4: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.668376]  remoteproc4: no firmware found
[   74.672700] rproc-user 2620050.dsp4: registered misc device dsp4
[   74.678995]  remoteproc5: 2620054.dsp5 is available
[   74.683888]  remoteproc5: Note: remoteproc is still under development and considered experimental.
[   74.692879]  remoteproc5: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.703293]  remoteproc5: no firmware found
[   74.707613] rproc-user 2620054.dsp5: registered misc device dsp5
[   74.713901]  remoteproc6: 2620058.dsp6 is available
[   74.718792]  remoteproc6: Note: remoteproc is still under development and considered experimental.
[   74.727782]  remoteproc6: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.738199]  remoteproc6: no firmware found
[   74.742524] rproc-user 2620058.dsp6: registered misc device dsp6
[   74.748831]  remoteproc7: 262005c.dsp7 is available
[   74.753724]  remoteproc7: Note: remoteproc is still under development and considered experimental.
[   74.762714]  remoteproc7: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[   74.773125]  remoteproc7: no firmware found
[   74.777449] rproc-user 262005c.dsp7: registered misc device dsp7
[   74.783495] rproc-user dspmem.10: kick gpio
[   74.787817] rproc-user dspmem.10: registered misc device dspmem
[   74.794004] ipip: IPv4 over IPv4 tunneling driver
[   74.799129] gre: GRE over IPv4 demultiplexor driver
[   74.804022] ip_gre: GRE over IPv4 tunneling driver
[   74.809639] TCP: cubic registered
[   74.812961] Initializing XFRM netlink socket
[   74.817823] NET: Registered protocol family 10
[   74.823383] NET: Registered protocol family 17
[   74.827851] NET: Registered protocol family 15
[   74.832351] Bridge firewalling registered
[   74.836375] 8021q: 802.1Q VLAN Support v1.8
[   74.842425] sctp: Hash tables configured (established 32768 bind 37449)
[   74.849428] NET: Registered protocol family 41
[   74.854013] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[   74.861714] Registering SWP/SWPB emulation handler
[   75.068834] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[   75.074351] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[   75.082743] xhci-hcd xhci-hcd.0.auto: irq 425, io mem 0x02690000
[   75.088836] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[   75.095648] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   75.102896] usb usb1: Product: xHCI Host Controller
[   75.107788] usb usb1: Manufacturer: Linux 3.10.72-rt77_BBM_V1.0.0 xhci-hcd
[   75.114687] usb usb1: SerialNumber: xhci-hcd.0.auto
[   75.120019] hub 1-0:1.0: USB hub found
[   75.123788] hub 1-0:1.0: 1 port detected
[   75.127908] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[   75.133418] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[   75.141173] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[   75.147984] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   75.155231] usb usb2: Product: xHCI Host Controller
[   75.160123] usb usb2: Manufacturer: Linux 3.10.72-rt77_BBM_V1.0.0 xhci-hcd
[   75.167020] usb usb2: SerialNumber: xhci-hcd.0.auto
[   75.172316] hub 2-0:1.0: USB hub found
[   75.176080] hub 2-0:1.0: 1 port detected
[   75.180448] UBI: attaching mtd2 to ubi0
[   78.761059] UBI: scanning is finished
[   78.764971] ai->vols_found 2
[   78.767856] ai->highest_vol_id 1
[   78.771089] ai->corr_peb_count 0
[   78.774322] ai->empty_peb_count 0
[   78.777641] ai->bad_peb_count 1
[   78.780786] ai->is_empty 0
[   78.783497] UBI error: ubi_read_volume_table: the layout volume was not found
[   78.793509] UBI error: ubi_attach_mtd_dev: failed to attach mtd2, error -22
[   78.800521] UBI error: ubi_init: cannot attach mtd2
[   78.809613] UBIFS error (pid 1): ubifs_mount: cannot open "ubi0:rootfs", error -19
[   78.817217] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0): error -19
[   78.825247] Please append a correct "root=" boot option; here are the available partitions:
[   78.833637] 1f00            1024 mtdblock0  (driver?)
[   78.838709] 1f01             512 mtdblock1  (driver?)
[   78.843783] 1f02         1047040 mtdblock2  (driver?)
[   78.848854] 1f03             512 mtdblock3  (driver?)
[   78.853927] 1f04           15872 mtdblock4  (driver?)
[   78.858999] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[   78.859003] CPU: 2 PID: 1 Comm: swapper/0 Not tainted 3.10.72-rt77_BBM_V1.0.0 #5
[   78.859028] [<c0015c48>] (unwind_backtrace+0x0/0xf8) from [<c0011cdc>] (show_stack+0x10/0x14)
[   78.859040] [<c0011cdc>] (show_stack+0x10/0x14) from [<c05192b0>] (panic+0x98/0x1f8)
[   78.859050] [<c05192b0>] (panic+0x98/0x1f8) from [<c074cfa8>] (mount_block_root+0x184/0x230)
[   78.859058] [<c074cfa8>] (mount_block_root+0x184/0x230) from [<c074d1f4>] (prepare_namespace+0x8c/0x18c)
[   78.859064] [<c074d1f4>] (prepare_namespace+0x8c/0x18c) from [<c074cc48>] (kernel_init_freeable+0x180/0x1c8)
[   78.859075] [<c074cc48>] (kernel_init_freeable+0x180/0x1c8) from [<c0512760>] (kernel_init+0x8/0xe4)
[   78.859081] [<c0512760>] (kernel_init+0x8/0xe4) from [<c000ddb8>] (ret_from_fork+0x14/0x3c)
[   78.859087] CPU3: stopping
[   78.859091] CPU: 3 PID: 0 Comm: swapper/3 Not tainted 3.10.72-rt77_BBM_V1.0.0 #5
[   78.859102] [<c0015c48>] (unwind_backtrace+0x0/0xf8) from [<c0011cdc>] (show_stack+0x10/0x14)
[   78.859110] [<c0011cdc>] (show_stack+0x10/0x14) from [<c0013f0c>] (handle_IPI+0xfc/0x160)
[   78.859115] [<c0013f0c>] (handle_IPI+0xfc/0x160) from [<c000858c>] (gic_handle_irq+0x54/0x5c)
[   78.859123] [<c000858c>] (gic_handle_irq+0x54/0x5c) from [<c051fd40>] (__irq_svc+0x40/0x84)
[   78.859125] Exception stack(0xee107f98 to 0xee107fe0)
[   78.859128] 7f80:                                                       00000003 00000000
[   78.859132] 7fa0: 00000a4e 00000000 ee106000 ee106000 ee106000 c07a7098 c07ffa30 c07ff25d
[   78.859136] 7fc0: c05274a0 00000000 00000000 ee107fe0 c000ef34 c000ef38 60000013 ffffffff
[   78.859142] [<c051fd40>] (__irq_svc+0x40/0x84) from [<c000ef38>] (arch_cpu_idle+0x28/0x30)
[   78.859151] [<c000ef38>] (arch_cpu_idle+0x28/0x30) from [<c005c830>] (cpu_startup_entry+0xa0/0x238)
[   78.859157] [<c005c830>] (cpu_startup_entry+0xa0/0x238) from [<80515ac4>] (0x80515ac4)
[   78.859160] CPU1: stopping
[   78.859163] CPU: 1 PID: 0 Comm: swapper/1 Not tainted 3.10.72-rt77_BBM_V1.0.0 #5
[   78.859173] [<c0015c48>] (unwind_backtrace+0x0/0xf8) from [<c0011cdc>] (show_stack+0x10/0x14)
[   78.859180] [<c0011cdc>] (show_stack+0x10/0x14) from [<c0013f0c>] (handle_IPI+0xfc/0x160)
[   78.859184] [<c0013f0c>] (handle_IPI+0xfc/0x160) from [<c000858c>] (gic_handle_irq+0x54/0x5c)
[   78.859190] [<c000858c>] (gic_handle_irq+0x54/0x5c) from [<c051fd40>] (__irq_svc+0x40/0x84)
[   78.859192] Exception stack(0xee103f98 to 0xee103fe0)
[   78.859195] 3f80:                                                       00000001 00000000
[   78.859199] 3fa0: 00001a0e 00000000 ee102000 ee102000 ee102000 c07a7098 c07ffa30 c07ff25d
[   78.859202] 3fc0: c05274a0 00000000 00000000 ee103fe0 c000ef34 c000ef38 60000013 ffffffff
[   78.859208] [<c051fd40>] (__irq_svc+0x40/0x84) from [<c000ef38>] (arch_cpu_idle+0x28/0x30)
[   78.859215] [<c000ef38>] (arch_cpu_idle+0x28/0x30) from [<c005c830>] (cpu_startup_entry+0xa0/0x238)
[   78.859219] [<c005c830>] (cpu_startup_entry+0xa0/0x238) from [<80515ac4>] (0x80515ac4)
[   78.859222] CPU0: stopping
[   78.859226] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.10.72-rt77_BBM_V1.0.0 #5
[   78.859236] [<c0015c48>] (unwind_backtrace+0x0/0xf8) from [<c0011cdc>] (show_stack+0x10/0x14)
[   78.859242] [<c0011cdc>] (show_stack+0x10/0x14) from [<c0013f0c>] (handle_IPI+0xfc/0x160)
[   78.859247] [<c0013f0c>] (handle_IPI+0xfc/0x160) from [<c000858c>] (gic_handle_irq+0x54/0x5c)
[   78.859252] [<c000858c>] (gic_handle_irq+0x54/0x5c) from [<c051fd40>] (__irq_svc+0x40/0x84)
[   78.859254] Exception stack(0xc079df68 to 0xc079dfb0)
[   78.859258] df60:                   00000000 00000000 00001640 00000000 c079c000 c079c000
[   78.859261] df80: c079c000 c07a7098 c07ffa30 c07ff25d c05274a0 00000000 00000000 c079dfb0
[   78.859264] dfa0: c000ef34 c000ef38 60000113 ffffffff
[   78.859270] [<c051fd40>] (__irq_svc+0x40/0x84) from [<c000ef38>] (arch_cpu_idle+0x28/0x30)
[   78.859276] [<c000ef38>] (arch_cpu_idle+0x28/0x30) from [<c005c830>] (cpu_startup_entry+0xa0/0x238)
[   78.859283] [<c005c830>] (cpu_startup_entry+0xa0/0x238) from [<c074ca70>] (start_kernel+0x300/0x358)
[   78.859288] [<c074ca70>] (start_kernel+0x300/0x358) from [<80008084>] (0x80008084)

 


Please help me sort out this issue. We struck here from many days.

 

With regards,

Yashavanth

  • Hi,

    The default u-boot env settings are as follows in include/configs/k2hk_evm.h:
          "args_ubi=setenv bootargs ${bootargs} rootfstype=ubifs "    \
        "root=ubi0:rootfs rootflags=sync rw ubi.mtd=ubifs,2048\0"

    Why do you deviate from this? Specifically: root=ubi0:rootfs rootflags=sync rw ubi.mtd=ubifs,2048?

    You set:
        root=ubi1:rootfs rootflags=sync rw ubi.mtd=2,2048

    Best Regards,

    Yordan

  • Hi yordan,

    Thanks for the reply.

    Sorry my mistake.  bootarg variable as:

    setenv args_ubi 'setenv bootargs ${bootargs} rootfstype=ubifs root=ubi0:rootfs rootflags=sync rw ubi.mtd=2,2048'

    You can see the bootarg print in bootlog is ubi0 not ubi1.

    With regards,

    Yashavanth

  • Hi,

    Can you try the following:
     

    Verify that the parameters you use when ubinizing the filesystem are correct.

    Also verify that you program your evm accordingly:
      

    Also check the FAQ in Linux User Guide:
      software-dl.ti.com/.../Foundational_Components_Kernel_FAQs.html

    Best Regards,
    Yordan

  • Hi yordan,

    I don't have problem in flashing. I got this issue only after changing my NAND size to 2GB before I was able to flash and boot. Because of our requirement we increased the size. Is any changes required with respect to nand driver code in kernel and uboot or any changes required in ubi image creation?

    Thanks and regards,

    Yashavanth

  • Hi,

    Seeing that you use kernel 3.10, I guess you use TI MCSDK Linux, right? I am not familiar with this release as it is quite old, but in Processor SDK Linux you should configure the nand in the aemif dts node in keystone-k2hk-evm.dts file and the same dts in u-boot.

    As for the ubi image creation, yes you should recalculate the parameters per your device physical eraseblocks, pages, subpages, etc.. This is described in the first link I've sent:

     

     There is a link called make ubifs in the UBIFS User-space tools section:
        

    Best Regards,
    Yordan