Part Number: AM5748
Other Parts Discussed in Thread: AM5728
Perf monitoring tool reports a 1 000 000% CPU utilization in Processor SDK Linux 6.0.0.7
Reproduce with the following command:
perf stat -a sleep 5
See the following two screenshots, first is on the 5.3.0.7 release and the second is on 6.0.0.7:
I know TI equipment is great and all, but for some reason I doubt a mere SDK upgrade would unlock an amazing 327 THz CPU on the AM5728_EVM board... ;)