This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5726: Clock definitions in U-boot

Part Number: AM5726


Hello,

I have made a custom board based of am572x-evm and beagleboard x15.

In the "u-boot"    ..  arch/arm/mach-omap2/omap5/hw_data.c

there are the clock definitions like

/* ABE M & N values with sysclk2(22.5792 MHz) as input */
static const struct dpll_params
abe_dpll_params_sysclk2_361267khz[NUM_SYS_CLKS] = {
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 12 MHz   */
{16, 1, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 20 MHz   */
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 16.8 MHz */
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 19.2 MHz */
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 26 MHz   */
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 27 MHz   */
{-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 38.4 MHz */
};

I think that comments are a little bit confusing, because wich clock source is used? It is the 20Mhz clock source on OSC0 or OSC1 ?

A few months ago I asked on this forum which clock sources is needed, the answer was the OSC1 were optional. https://e2e.ti.com/support/processors/f/791/t/743176

On my custom board I don`t use the OSC1!

I tought that the sysboot pins 8 and 9 would indicate after starting up the processor which clock speed is selected for SYS_CLK1 (OSCO0).

Trough the SYSBOOT8/9 it is only possible to select 4 clock speed but in the structure there are 7 defined.

There are a general equation for the clocks?

for example to calculate the clock for structure "core_dpll_params_2128mhz_dra7xx"

I get 2128 MHz if I calculate 266MHz / 4  * 2 * 1

-> OSCO{1,2}  *  m / n * m2 * m3 ?

And what about structure static const struct dpll_params per_dpll_params_768mhz[NUM_SYS_CLKS

is that calcultion correct?

16.8 Mhz * 160 / 6 * 4 * 3 * 6 * 4 * (2+1) ???

I dont get the expected 768Mhz just only 774 Mhz what is wrong?