Part Number: AMIC110
Other Parts Discussed in Thread: TLK105, DP83822I
Tool/software: Code Composer Studio
Dear Sir/Madam,
we have an AMIC110 ASIC with PRUICSS EtherCAT and two DP83822 phys connected. We are developing an EtherCAT application without synchronisation (Distributed Clocks). We have based our application on the "ethercat_slave_full_AMIC11x_arm" example application. As far as we can see at the moment, EtherCAT seems to be running. The problem we have at the moment is that with the PDI Watchdog activated we can not go to OP. The reason is that the PDI watchdog does not seem to be triggered.
We have changed the trigger mode to PDI_WD_TRIGGER_RX_SOF from PDI_WD_TRIGGER_LATCH_IN (we have no digital outputs) but there is no improvement.
The PDI interrupt is OK (2ms with twincat).
Can you please explain how this is supposed to work?
Is there a way to diagnose why the watchdog is not triggered?
Thank you
Best Regards
Falk Bastille