Part Number: AM3358
Hello team,
I have designed a custom board using AM3358.
In one of the boards I have found that processor is not booting.I have checked the UART log and even CCCCC.... was not coming.
So, I tried connecting the board using CCS(Code Composer Studio) and found the following error.
CortxA8: Output: **** AM3358_SK Initialization is in progress ..........
CortxA8: Output: **** AM335x ALL PLL Config for OPP == OPP100 is in progress .........
CortxA8: Output: Input Clock Read from SYSBOOT[15:14]: 24MHz
CortxA8: Output: **** Going to Bypass...
CortxA8: Output: **** Bypassed, changing values...
CortxA8: Output: **** Locking ARM PLL
CortxA8: Output: **** Core Bypassed
CortxA8: Output: **** Now locking Core...
The board is stuck at locking the core.
I have verified the voltages of CAP_VDD_SRAM_CORE,CAP_VDD_SRAM_MPU,CAP_VBB_MPU.
I have also verified the reset oins of processor and processor is not in the Reset mode.
I could sense some voltage is not being properly connected and is causing issue. If i am sensing correct , Kindly help me in identifying the issue and solving it.
Else let me know what could be the issue.
Kindly reply at the earliest.
Regards
Mad_hu