This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF89: Blaun to support low frequency insted of the TCM3-452X-1+

Part Number: DAC38RF89


Hello,

I would like to use the DAC38RF89  in the frequency range of  1MHz–35MHz

 The recommended Balune TCM3-452X-1+   does not support this band.

Can you reccomend other balun.

*The DAC38RF89   is mandatoty and could not be change because I'm using it also for .20MHz-3500MHz Band.

Thank you