Part Number: TRF372017
Other Parts Discussed in Thread: LMX8410L,

The question is : Should I follow the rule of datasheet or the action of EVM?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRF372017
Other Parts Discussed in Thread: LMX8410L,


Hi,
FYI, please refer to the following E2E as a reference:
Q1. How to export register list from GUI for TRF372017?
you may press save register to file button on the GUI.

Q2. What is the sequence of registers? (Reg. 5 -> Reg.4 -> Reg.3 -> Reg.2 -> Reg.1)
There is no specific sequence to the register writes to the TRF372017. Please be sure to trigger EN_CAL at the end of the process. See previous E2E post for detail on the programming sequence
There are 7 Registers, but why only capture 5 Register from LA?
you should see 7 registers being exercisable by the GUI. You can try to change the values of register 6 and 7 and observe the output. Register 6 and 7 are trim adjustments for DC correction and or performance, therefore, they are not written all the time.
Q4. As datasheet mention, CSB needs pulling high before write register and do it again after finish writing.So there should be twice pull high for CSB, but only capture the "finish" one from EVM.
The LE in the datasheet is to latch in the previous SPI write. Therefore, you should follow the datasheet if you are doing continuous writes. See datasheet instruction below
"The LE is asynchronous to the CLOCK and at its rising edge the data in the shift register gets loaded onto the selected internal register"