Part Number: TRF372017
Other Parts Discussed in Thread: DAC3484
I have a question regarding the TRF37201 VCM.
The datasheet indicates that when using the internal VCM, the BB input should be AC coupled. In this case TRF37201 settings would be the following:
PWD_BB_VCM=0
VREF_SEL_n=0~7(Default 4)
If using Offset adjustment
PWD_DC_OFF=0
IOFF_n=0~255(Default 128)
QOFF_n=0~255(Default 128)
If the VCM is generated externally, the datasheet only shows a sample circuit that uses the BB input with DC coupling, with a description of setting the VCM to 1.7V, but there is no description of the IC settings.
Could you provide the settings for PWD_BB_VCM and PWD_DC_OFF when VCM is supplied externally?