This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for RF Generator Power Supply Driver, and RF Generator



I'm looking to connect a power supply to a RF generator in series and then attached to a copper coil. Power input to the coil needs to be ~300W at ~0.88 MHz. Full Schematic is shown below.

  • Tyler,

    Cool system schematic you've attached. It looks as if you originally submitted this question into the RF & Microwave Forum but it's been routed into the Power Management Forum. The HV power supplies shown in your block diagram are interesting nd this is the area I may be able to help with.
    You've already provided some specs on the system but do you have any electrical specifications for the HV power supplies you can share? VIN, VOUT, POUT, Isolation, desired switching frequency, etc?

    Regards,

    Steve M

  • We already have the HV PS being supplied by the test facility and we have our own as back-up. They are very high voltage, low current DC.

  • Tyler,

    Great to hear you are all set on the power side. I believe the way you phrased your question, beginning with: "I'm looking to connect a power supply..." is probably how your post was redirected from RF & Microwave to Power Management. I might suggest you repost in the RF & Microwave again but with more specific detail about the help needed. Thanks for posting in E2E and good luck with your design.

    Regards,

    Steve