This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7700: IQ Mismatch Cal not working

Part Number: AFE7700


I'm using an AFE7700EVM with LATTE lib 20.1. The AFE7700 is configured in mode2 (RX=TX=FB=245.76Msps). The JESD lanes are UP.

I have looped back TX1 on FB1 with a bandpass filter.

The board is connected to a ZCU102 and a NCO inside the FPGA is generating a CW tone.

I'm not able to execute the TX QMC Calibration.

Nothing is happening on the output signal when I execute the following command: AFE.TOP.TIMINGCTRL.txToFbSelectCh(1,0)

- Is there additional functions to check whether it started or not ? (or what the problem is)

- What signal should be generated by the FPGA for the calibration?

Thanks

Robin