This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm Using the DAC38RF89I and wanted to know what is the best way to place the BALUN peripherals.
For mechanical issues I can't use parts in the Print side (P.S) with thickness bigger then 0.3mm, so the inductors could be only in the BALUN side (C.S).
I saw the in the EVB the differential lines are "open" near the BALUN, is that OK ?
I wanted to know if my way is also good. (See PIC bellow).
Thanks
Ronen
TI EVB BALUN Input
ELBIT BALUN Input
Hi Ronen,
Yes, your configuration of the balun connections should be fine. Please make sure those output traces are symmetrical in length.
Regards,
Rob