Other Parts Discussed in Thread: THS4303, THS4304, , TL081, LMH6521, LMH6523, LMH6554, LMH2832, LMH6881, OPA857, TINA-TI, BUF802
Hello there,
I am willing to buy THS4302, THS4303, THS4304 op-amps. I came across with few problems listed below:
1. The PSpice model downloaded from the official website of TI is not compatible with the ADS simulator.
2. When I'm trying to simulate a circuit based on a THS4302 operational amplifier with the ADS simulator. I'm using the official PSPICE model downloaded from:
Unfortunately, it seems that it doesn't work due to compatibility issues.
Error detected by hpeesofsim during netlist flattening. 'ths4302.sbias' is an instance of an undefined model 'spice_vswitch'.
3. The PSpice model pin configuration of THS4302,THS4303,THS4304 is not available in datasheet. The Datasheet should contain pin specification that which terminal is input and output pins etc. then only end-user will be able to simulate the circuit.
For your reference, The Datasheet of op-amp TL081(taken from the TI website) is having pin configuration.
Can you please clarify my doubt as soon as possible