Other Parts Discussed in Thread: LMK04828
The DAC output is 1100MHz. There are spurious of 1M and 37.5M, respectively.
The PLL configuration of the DAC is as follows:0x31 0x0400;0x32 0x0508;0x33 0x2A24.
The DAC clock is 200MHz of differential input.The VCO frequency is 4800MHz.
I can't find the source of the spurious at the moment, I hope you can give me some inspiration.
Thanks,
Yunlong.