Part Number: AFE7769EVM
Other Parts Discussed in Thread: AFE7700, AFE7769, AFE7700EVM, AFE7900, AFE7950
hi,
Comparing the two datasheets (AFE7769 Vs AFE7700), I do not find the technical difference but just the applications. TI explicitly says that the AFE7700 is for vector signal transceiver, which is exactly what I need to build a multiple-port VNA working at the frequency about several hundred MHz to 2 GHz). Could you help to list the main difference between the two?
I kind of prefer to use AFE7700EVM. But I cannot find many supporting documents from TI website. I only can find the user guide for AFE7700EVM so far.
I am planning to use either one with TSW14J57EVM (with Intel's Arria 10), which is the most suitable choice?
Best regards,
Felix