This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: how use External clock mode?

Part Number: AFE7950EVM
Other Parts Discussed in Thread: LMK04828

I want to use the external clock mode on the AFE7950EVM.

    Fref 11520MHz, FadcRx 2880MHz, FDac 11520MHz

I changed the AFE7950EVM hardware and Latte

1> hardware 

Remove R372, R373, R368, R369
Insert R370, R371, R366, R367, L40, L41

Insert C80, C81

2> Latte

setupParams.skipFpga = 1

sysParams = AFE.systemParams

setupParams.fpgaRefClk = 180

AFE.systemStatus.loadTrims = 1

sysParams.externalClockTx = True

sysParams.externalClockRx = True

sysParams.FRef = 11520

sysParams.FadcRx = 2880

sysParams.FadcFb = 2880

sysParams.Fdac = 11520

## The following parameters sets up the LMK04828 clocking schemes

lmkParams.pllEn = True

lmkParams.inputClk = 2880

lmkParams.sysrefFreq = 0.06

lmkParams.lmkFrefClk = False

Message printed by Latte after run

    Couldn't get the link up for device RX: 1; Alarms: 0xbfc0

    Couldn't get the link up for device RX: 1; Alarms: 0xbfc0

more settings to add???