Other Parts Discussed in Thread: AFE7900, , AFE7950EVM, AFE7950
Hello Support Team,
Below are the queries regarding AGC mechanism for AFE79XXEVM. Please guide.
1. Analog , digital peak detectors are inbuilt in the AFE7900 and when we use internal AGC controller, it is used for below as per my understanding.
- Peak the main RF input power level through internal Analog RF peak detector.
- Sets the specific internal DSA settings as per ADC input range requirement.
As my input dynamic range is high, so I also need to use external VGA to support weak signals to fall into the ADC range, So, Is it possible to control the external VGA through internal AGC controller via GPIO pins? in that way, the internal DSA as well external VGA/DSA can be automated irrespective of the input RF signal range?
2. digital gain compensation function is used to compensate all the attenuation settings , gain provided in between the RF input to JESD output, right? So, it also compensate all the DDC mixer losses affected the input signal's amplitude?
3. If input power is unknown and I want to measure the actual power input in the digital domain, So, I think It is possible to correlate the analog peak detector output to AGC and the total gain compensation made throughout the chain, Can you please suggest ?