Part Number: AFE7900EVM
Other Parts Discussed in Thread: AFE7900
Hello,
I am planning to use AFE7990EVM with ZCU102 FPGA Evalutaion board. My input frequency is not a fixed frequency. It will be inside a range and will vary based on the requirement inside the applicable frequency range.
So, By using AFE7900VM DDC , So, based on my input RF frequency, NCO selection needs to be done to generate baseband I , Q.
So, every time based on change in my RF input frequency, Do I need to manual change of NCO frequency or Is there any way ( by using Latte) to change the NCO frequency based on the input RF frequency to generate I.Q.
For example, Input RF = 30 MHz with bandwidth = 1 MHz, NCO FREQ. requirement = 30 MHz and generation of I,Q by using decimation filters . Now my input RF frequency is being changed to let's say 50 MHz and now NCO freq setting requirement = 50 MHz to generate baseband. So, Is it possible to make an implementation in latte , to change the NCO frequency same as RF input frequency to generate I,Q ?
As NCO is programmable, so, basically, I want to make NCO programmable with respect to input frequency range to generate constant baseband I,Q. For which there has to be one logic that change the NCO frequency same based on input RF frequency.
Awaited your support and guidance on the above,