Hi
The AFE7950 has three SPI ports (SPIA, SPIB, and SPIB2)
With only SPIA connected, is it possible to set AFE7950 with LATTE?
When using only SPIA, is there any setting required for LATTE?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The AFE7950 has three SPI ports (SPIA, SPIB, and SPIB2)
With only SPIA connected, is it possible to set AFE7950 with LATTE?
When using only SPIA, is there any setting required for LATTE?
Hi JB,
SPIA is the main SPI interface and you can program the AFE using only SPIA. When using Latte and the AFE7950EVM we are only using SPIA for programming. This is set by default and no additional changes are needed.
Regards,
David Chaparro