In TI tranning, I have some quetions about radar equation.
Intro to mmWave Sensing : FMCW Radars - Module 4 : Some System Design Topics | TI.com Video
1)
Total meausrement time (called as integration time or active frame time) is N*Tc.
After range-FFT and Doppler-FFT, the processing gain is N*Tc.
Is the processing gain is Tc if range-FFT is only passed ?
2)
The processing gain means the gain obtained after ADC output.
If target is located at far range and ADC input SNR is very low about ~0dB (inability to distinguish between signal and noise), can the target be detected when processing gain is increased by increase of measurement time?
Is it possible to detect a far range target if the total measurement time is increased?