Part Number: LMX8410L
Other Parts Discussed in Thread: LMX2594
I have a close circuit application of LMX8410, where the LO output is used to drive a separate upconverting I/Q mixer, whose output is looped back somehow to the LMX8410. The main LO frequency is around 6HGz, so I need to use the div2 mode of the I/Q generator.
The problem is, when the LO is effectively set to different frequencies around 6HGz, the LO output appears to have random times of 90 degree shift from the LMX8410 internal mixer LO. And in my application, I can see I/Q swap and shift accordingly. I understand that LO output can use the VCO channel divider and the div2 mode of the I/Q generator has its own divider, so there can be such misalignment.
From the datasheet, I gathered the LO output can be synchronized to the SYNC signal and the mixer can only synchronize to SYNC when the frequency is whole times of Fosc, which is not always the case in my application. However, I realize the the R80 register seems to address the mixer LO sync issue, especially the control bit of SYNC_PHASE_MIXLO Sync bit to close the loop from Mixer LO back to synthesizer looks promising.
Is it possible to sync the LO output to the mixer under div2 mode, for example at 6.000001GHz when the Fosc is 0.1GHz? and any chance to know more details about how to use the SYNC_PHASE_MIXLO control bit?
Many thanks,
David