Part Number: DAC38RF80
Hello,
I am trying to understand the operation of the NCO in a DAC38RF80 as shown in Figure 66 on document SLASEA3C,
1) What is the mapping between the 48 bit accumulator output and the 16 bits used to index into the lookup table, ie are the least significant (LS) or the most significant (MS) 16 accumulator bits used?
I have seen another TI DAC with a 32 bit accumulator. What is the advantage of 48 bits over 32?
2) The lookup table outputs are 16 bits wide, but it is a 14 bit DAC. Are the extra bits used to increase the internal accuracy when combining sin and cos to make the output, with the 14 MS bits of that calculation used at the output?
3) Changing the interpolation rate (using the GUI on the EVM) changes the output frequency. What is the mechanism there? Fig 66 does not indicate any interpolation effects.